2024-02-12 2:44 AM
Hello, I am working with STM32WBA52CG as a central and I want to read the RSSI from the incoming advertising packets. The RSSI value should be a negative value in dBm, however it is defined as uint8_t in the AdvertisingReport_t structure. Can someone explain me how to get the correct RSSI value? I am getting the values shown on the terminal below.
...
}
bleAppContext.BleApplicationContext_legacy.connectionHandle = p_conn_complete->Connection_Handle;
GATT_CLIENT_APP_Set_Conn_Handle(0, p_conn_complete->Connection_Handle);
/* USER CODE BEGIN HCI_EVT_LE_CONN_COMPLETE */
/* USER CODE END HCI_EVT_LE_CONN_COMPLETE */
break; /* HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE */
}
case HCI_LE_ADVERTISING_REPORT_SUBEVT_CODE:
{
hci_le_advertising_report_event_rp0 *p_adv_report;
p_adv_report = (hci_le_advertising_report_event_rp0 *) p_meta_evt->data;
UNUSED(p_adv_report);
/* USER CODE BEGIN HCI_EVT_LE_ADVERTISING_REPORT */
uint8_t rssi = p_adv_report->Advertising_Report[0].RSSI;
LOG_INFO_APP("RSSI from struct: %d , ", rssi);
/* USER CODE END HCI_EVT_LE_ADVERTISING_REPORT */
break; /* HCI_LE_ADVERTISING_REPORT_SUBEVT_CODE */
}
...
2024-02-12 2:47 AM
What does the documentation tell you?
2024-02-12 2:51 AM
The RSSI parameter in the AdvertisingReport_t structure is defined in this way. It is defined as uint8_t but it should be a negative value.
...
/**
* RSSI (signed integer).
* Units: dBm.
* Values:
* - 127: RSSI not available
* - -127 ... 20
*/
uint8_t RSSI;
} Advertising_Report_t;
2024-02-12 2:57 AM
The RSSI parameter in the AdvertisingReport_t structure is defined in this way. It is defined as uint8_t but it should be a negative value.
/**
* RSSI (signed integer).
* Units: dBm.
* Values:
* - 127: RSSI not available
* - -127 ... 20
*/
uint8_t RSSI;
} Advertising_Report_t;
2024-02-12 3:09 AM
As far as transporting it over the air, it's just a byte.
When it comes to using it, cast it to int8_t ?
Take a look a the chip documentation - does that give any clues?
2024-02-12 3:14 AM
If it is just a byte, a value such as 74 does not make sense. As per chip documentation there is no clear information about this RSSI value interpretation.
2024-02-13 7:39 AM
Hi Portilha
In fact, the structures of the type "hci_le_advertising_report_event_rp0" mapped to the RAM buffer were not designed to do this.
For the RSSI, you need to use the following macro:
==>ble.h:
/* Exported macros -----------------------------------------------------------*/
/* -------------------------------- *
* [retrieved from ble_legacy file]
* Macro to get RSSI from advertising report #0.
* "p" must be a pointer to the event parameters buffer
* -------------------------------- */
#define HCI_LE_ADVERTISING_REPORT_RSSI_0(p) \
(*(int8_t*)((&((hci_le_advertising_report_event_rp0*)(p))-> \
Advertising_Report[0].Length_Data) + 1 + \
((hci_le_advertising_report_event_rp0*)(p))-> \
Advertising_Report[0].Length_Data))
==>app_ble.c :
int8_t rssi = HCI_LE_ADVERTISING_REPORT_RSSI_0(p_meta_evt->data);
Clarifications will be added to the code regarding this subject in the upcoming releases.
BR, Joé
2024-02-14 1:17 AM
I have exported that macro to file "ble.h" and I am using it on the SVCCTL_App_Notification function in file "app_ble.c", however the RSSI value keeps returning 0 all the time. Can you clarify?
...
case HCI_LE_ADVERTISING_REPORT_SUBEVT_CODE:
{
hci_le_advertising_report_event_rp0 *p_adv_report;
p_adv_report = (hci_le_advertising_report_event_rp0 *) p_meta_evt->data;
UNUSED(p_adv_report);
/* USER CODE BEGIN HCI_EVT_LE_ADVERTISING_REPORT */
int8_t rssi = HCI_LE_ADVERTISING_REPORT_RSSI_0(p_meta_evt->data);
LOG_INFO_APP("RSSI %d\r\n", rssi);
// parse_advData(&p_adv_report->Advertising_Report->Data, p_adv_report->Advertising_Report->Length_Data, p_adv_report->Advertising_Report->Length_Data,
// &p_adv_report->Advertising_Report->Address, rssi);
/* USER CODE END HCI_EVT_LE_ADVERTISING_REPORT */
break; /* HCI_LE_ADVERTISING_REPORT_SUBEVT_CODE */
}
...
2024-02-14 7:54 AM
What version of MCU Package are you using? The v1.0.0?
Have you tried starting from a release app and only adding these modifications to it?
2024-02-14 7:59 AM
I am using the Firmware version 1.2.0, according to STM32CubeIDE. What do you mean by starting from a release app? I am using the BLE project examples provided by ST like P2PServer, P2PClient, etc.