cancel
Showing results for 
Search instead for 
Did you mean: 

120mA current consumption when supply external 3V3 power - Nucleo-WL55JC1 (CN6)

digidhamu
Associate III

When you power Nucleo-WL55JC! with external 3V3 via CN6, I could see constant 120mA current consumption. Is there any way we can reduce this?

6 REPLIES 6
digidhamu
Associate III

I have tried removing 5V_PWR jumper JP7 and no jumpers on JP4 as per the documentation but no luck

Louis AUDOLY
ST Employee

Hello,

Can you tell me which program you are using to reproduce your behavior please.

Have a nice day

Regards

LoRaWAN_End_Node application provided by ST under this path

Projects/NUCLEO-WL55JC/Applications/LoRaWAN/LoRaWAN_End_Node

Thanks LAUDO and wait for your advise.

Is there any update on this @Louis AUDOLY​ as I waiting to solve of my use cases

Louis AUDOLY
ST Employee

Hello @digidhamu​ ,

Sorry for the late reply

I tested the power consumption of a nucleo board with the end_node project and my consumption were around 20mA when we did a Tx and a below 200uA when nothing happen.

Don't you have any expansion board connected to the nucleo ?

Best regards

Thanks @Louis AUDOLY​ I didn't connect any expansion board. Would it possible to send picture of your setup and this will help me to report you back faster?