2023-09-18 7:32 AM
Hi Guys
How on earth does ST expect anyone to use, learn and embrace their products when there seem to be so little help , videos training??
TouchGFX is appalling for step by step examples, YES it's free, but no value to engineers if you have no idea or can't understand Toucgfx
I have been days traying to create an event from a custom container with a toggle switch
under the container I have created an event for a toggle button
I have called the container panel which holds the toggle button and event
under generated gui I see the generated event handler
I then want to copy that event handler in to panel.cpp and create a new event for a custom container
The compiler just errors every time ????? I ready to lunch the PC
There must be a better easier way than touch GFX, im sure its great if you know what on earth you are doing
2023-09-18 9:34 AM
I mean here is all or 80% what you need TouchGFX Documentation | TouchGFX Documentation
2023-09-18 11:58 PM
I disagree with the 80%. The majority of the documentation is auto-generated. Look at their API documentation and see if you can figure out how to use a particular class from it. Some yes, most no. For example, how do you use the Gradient class?
2023-09-19 12:43 AM
I simply think Touchgfx is great program and design tool, but very little time and effort has been giving to good structured training and examples. You need an online training cource to teach you and show you the way with every aspect of touchgfx, you can't be bumming arround for three days trying to get a button click event in a custom container!!
Its clear the program has great potential, shame about the lack of examples and guides, there needs to be 100s and 100s of Easy Step By Step examples, clearly showing every stage, so the engineer can understand and get it!!
Thats if you have not launched the PC first out of anger from the compiler errors that make no sense
2023-09-19 1:12 AM
this type of page is so unhelpful ???
There should be 5 or 6 examples at the bottom showing how the click listner works ????/
the pages really mean nothing to me, very dificult to understand and no help at all >???
????????????????????????????????????????????????????????
2023-09-19 2:39 AM - edited 2023-09-19 2:40 AM
Hello.
You dont need to make buttonCallbackHandler by yourself to panel-class. Just add ev and JIMJIM- functions to panel class. Tgfx generates calls to those automatically to the panelbase- class. You found empty declations in panelbase.hpp file for those functions, just copy/modify those to the panel.hpp/.cpp
There is also example about simple button operation. Open tgfx designer and select examples on the left menu. I guess these examples are good way to learn how to use different widgets. You can select simulator as target board if you just want to test different examples.
Hope you get forward, and ask more if needed.
Br J.T