2022-08-01 01:36 AM
2022-08-01 02:00 AM
In addition to the above question: I noticed that the screen Screen1View is deleted from the drive somehow but, the Screen1Presenter is present. It's not in the recycle bin. I'm still working to fix it without developing a new 5 page UI.
2022-08-01 08:21 PM
To All,
I could not resolve my issue. However, thanks to the container property in Touchgfx and saving previously written code in advance, I managed to recreate the screens with code without any problems.
What I'm going to do from this point on is save a copy of the entire project. Let's see if it helps.
Thanks,
Hiram
2022-08-08 02:41 AM
Hello @Hiram Hyman ,
Nice to hear that you found a solution to your problem.
Let us know if you have other issues with your project.
/Yoann