cancel
Showing results for 
Search instead for 
Did you mean: 

UnmappedDataFont compile error

GMeur
Senior II

Hello,

I'm using the version 16.1 of TouchGFX and when I generate the project on the simulator I get these error messages when I try to run the code in VS :

0693W00000QMlcFQAT.pngI generate the project with the following text config:

0693W00000QMlcKQAT.png 

Any help is more than welcome.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Yoann KLEIN
ST Employee

Hello @GMeur​ ,

To be sure, did you already try to generate code with TouchGFX 4.20.0 ?

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX