Using touchgfx without external RAM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-18 2:24 AM
I designed a GUI on stm32f746 discovery board and programmed the board successfully and GUI worked perfectly, now I want to redesign the GUI and my programm to be able to use a custom board which doesn't have an external RAM
at first I disabled the MX_FMC_Init fuction but the display is black and nothing shows up, then I read the article below and followed the instruction but display went black again.
I'm a beginner and I would be very gratefull if anyone guides me how to config the CubeMX and touchgfx to work without external RAM.
https://support.touchgfx.com/docs/development/board-bring-up/how-to/03-display-internal
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-22 3:05 AM
O now I get what you meant,
I made these changes you mentioned in touchGFXGeneratedHAL.cpp file, but the output is the same :(
extern uint16_t framebuffer[400*100*3];
void TouchGFXGeneratedHAL::initialize()
{
HAL::initialize();
registerEventListener(*(Application::getInstance()));
registerTaskDelayFunction(&OSWrappers::taskDelay);
setFrameRefreshStrategy(HAL::REFRESH_STRATEGY_OPTIM_SINGLE_BUFFER_TFT_CTRL);
setFrameBufferStartAddresses((void*)framebuffer, (void*)0, (void*)0);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-22 8:37 AM
How you build your project? Because when in TouchGFX, then generated files is overwrited on each build. Your changes is removed.
I recommend use IDE . and you dont write where yuo place line in main?
HAL_LTDC_SetAddress(&hltdc, (uint32_t*)framebuffer, LTDC_LAYER_1);
As simple test add memset(framebuffer,55,4800); //this make some gray part on screen when buffer works.
Too i recomm use debuger and check if your code work and not halt in an hardfault...
Why 400*100*3 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-24 2:56 PM
Hi @ETale.1​
May be it is now too late to post an answer
I was also looking to use Touchgfx without external RAM as my application has very minimal graphics. This post helped me a lot to poke at the right places
Here is what I did
- Open Cube MX configurator
- Change to single buffer and by allocation
- This would update TouchGFXGeneratedHAL.cpp as described in here Framebuffer Strategies | TouchGFX Documentation
- What they dont post is that there is another file TouchGFXHAL.cpp which is not generated and overrides whatever was changed in the base TouchGFXGeneratedHAL class
- So, we need to comment out the following two lines in the TouchGFXHAL.cpp file below
void TouchGFXHAL::initialize()
{
// Calling parent implementation of initialize().
//
// To overwrite the generated implementation, omit call to parent function
// and implemented needed functionality here.
// Please note, HAL::initialize() must be called to initialize the framework.
TouchGFXGeneratedHAL::initialize();
// Commented out
// setFrameBufferStartAddresses((void*)0xC0000000, (void*)0xC003FC00, (void*)0xC007F800); //enable the animation storage to allow slide animations
// lockDMAToFrontPorch(false);
instrumentation.init();
setMCUInstrumentation(&instrumentation);
enableMCULoadCalculation(true);
}
- Now, you have to modify the linker files and create a section named 'TouchGFX_Framebuffer' which is the name used by the code generator
- Modify STM32F746NGHX_RAM.ld
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
// frame buffer is 255k long in my case
RAM_FRAME_BUFFER (xrw) : ORIGIN = 0x20001000, LENGTH = 256K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
}
// add at the end
/*Added for frame buffer */
.TouchGFX_Framebuffer : {
__TouchGFX_Framebuffer_start = .;
KEEP(*(.TouchGFX_Framebuffer))
__TouchGFX_Framebuffer_end = .;
} > RAM_FRAME_BUFFER
- Clean and build
Thanks,
Vimal
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-24 9:51 PM
I am interested as well to know this. Would choosing partial framebuffer help in this case?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-24 11:32 PM
Hi,
Could you maybe add in the "Idea zone" of this forum the demand of improvement of this article ? It makes sense to put a reminder that due to the hierarchy of the code the generated files can be overwritten by the user in the relevant files.
/Romain
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-25 7:13 AM
Partial is usable only when LCD have own memory framebuffer. And too partial cant use acceleration. And one example of custom 1280x480 LTDC layer 0 image in flash, 1024x320 layer 1 320kB (internal ram) TouchGFX framebuffer with alpha 150.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-11-28 11:19 PM
hi ETale.1
are you got any solution
i am also stuck in same problem

- « Previous
- Next »