2024-02-08 06:47 AM
Hello,
I have a problem with a STM32U5G9J-DK2 :
If I choose a project with FreeRTOS in GFX designer, I can upload the code in my board from GFX designer : it does work.
If I open the project file with CubeMXIde, I can modifiy and then upload the code in my board : it does work.
If I choose a project with Azure RTOS ThreadX, I can upload the code in my board from GFX designer : it does work.
But
If I open the generated project with Azure RTOS ThreadX in CubeMXIde, when I build the project, I have some undefined references, even if I do no modification of the generated code : it does not work.
It seems that I have a problem with the file HardwareMJPEGDecoder.hpp or .cpp but I am far to be certain.
I would like to know if it is a well-know and easy problem to solve with this lack of information
or more information is necessary ?
Thank you
Kind regards
David
Solved! Go to Solution.
2024-02-09 01:25 AM
Hello Osman,
Thank you very much for your very fast and efficient answer.
It works.
I haden't thought to do that but I am very new with TouchGFX and RTOS.
I have received my board yesterday and I was a little bit lost...
Have a good day
Kind regards
2024-02-08 07:48 AM
Hello @davidzuercher ,
This is correct, there's indeed an issue with this TBS. We apologize for the inconvenience. We'll fix this TBS as soon as possible but meanwhile, to remove that bug, you can regenerate code on STM32CubeMX (and then regenerate code in TouchGFX again). I'll get back to you when it's fixed.
2024-02-09 01:25 AM
Hello Osman,
Thank you very much for your very fast and efficient answer.
It works.
I haden't thought to do that but I am very new with TouchGFX and RTOS.
I have received my board yesterday and I was a little bit lost...
Have a good day
Kind regards
2024-02-09 02:39 AM
Hello @davidzuercher ,
We fixed that issue this morning. You need to delete this folder bellow, and reopen TouchGFX Designer to apply our fix:
C:\Users\YOUR_USER_NAME\AppData\Roaming\TouchGFX-4.23.1\Downloads\STM32U5G9J-DK2
By the way, welcome to the TouchGFX Community, please feel free to reach us out if you need help in your application development. I can recommend you to have a look to our documentation site if you're new to TouchGFX