2022-03-03 9:30 AM
We are considering a custom PCB design similar to the STM32H743I-EVAL.
However, we just discovered that when creating a TouchGFX project for this board, many configured pins are set different (shown in STM32CubeMX) than given on these schematics:
https://www.st.com/resource/en/schematic_pack/mb1246-b0x_schematic.pdf
https://www.st.com/resource/en/schematic_pack/mb1246-e02_schematic.pdf
A few examples of signales routed to other pins for the SDRAM: SDNWE,SDNE1, SDCEK1. There are also a handful of pins for the LCD which are routed elsewhere. The TouchGFX project runs fine so obviously these schematics must be invalid..
Is there a newer schematic version than MB1246-E02 dated in 2019?
Many thanks in advance
2022-03-03 9:37 AM
There have been several versions of the board what one do you actually have?
The Rev E is EVAL2, with the ST-LINK/V3
2022-03-03 10:03 AM
The board has STLINKV3 and the printed label on the MCU board says: MB1246-H743XI-E02, which should indicate it has the second schematic in my post. The display board says MB1063 REV B.
However, I can't find any other schematics than listed above
2022-03-03 11:49 AM
Right, but that's their prerogative, you might have to talk to an FAE to get others.
You might want to cross check the BGA ball assignments, I recall there being some subtle changes in a handful of them over the development cycle for the H7's which spanned back to 2017
Also the EVAL boards tend to have a myriad of solder-bridge and resistor paths to remap or reconfigure board use cases.
2022-03-04 1:46 AM
You are right, there is a myriad of solder bridges on this board but nothing shown on the schematics above that would allow balls assigments they way TouchGFX does.
@ST representatives, could you please help me out finding the right version of the schematic? If no schematic is available, please let me know also. (post this elsewhere?)
Thanks
2022-03-07 6:25 AM
Hi @Lars Sörqvist ,
I got the confirmation that the schematic version of April 2019 for MB1246-E02 is the latest one.
So we need the help of our Experts from TouchGFX team (@Romain DIELEMAN & @Alexandre RENOUX ) to understand more how TouchGFX matches STM32H743I-EVAL hardware design.
In all cases, for your pcb setup, references are the product datasheet and the application note about the hardware getting started.
You can also have a look to the user manual UM2198 Evaluation boards with STM32H743XI and STM32H753XI MCUs to check the main updates of the hardware revisions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-03-07 6:58 AM
Hi Amel!
Many thanks for helping out -:)
I believe my MB1246-E02 schematic is dated 13th Feb. 2019 and not April. Is there a link to a newer schematic verison?
In any case, I'll await some hints from your collegues about the matching TouchGFX (BGA pins) vs. schematic for this board.