cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX Analog Clock example runs slow on STM32H747I DISCO

Kenwang
Associate III

I executed "Clock Example" on stm32H747I DISCO. I found that after two minutes of execution, the analog clock was about 15 seconds slower. After 53 minutes of execution, it was about 5 minutes slower, and it will become slower and slower. I did not add any The program code is in the M7 core. The way I compare is to enable RTC and uart in the M4 core, use the HAL_RTC_GetTime() function to read out the rtc time every second, and print it out through the uart. My question is, If the analog clock really slows down, is there any way I can correct it without users noticing?

12 REPLIES 12

Hello @Kenwang,

I tested the example on the simulator and didn't experience the clock slowing down. In addition, I don't understand why you decided to increase the priority of videoTask since it is not responsible for animations. 

Following the suggestions given by our lovely friends would be a good solution to ensure the clock won't fall behind. 

Best regards,

Mohammad MORADI
ST Software Developer | TouchGFX

Primary understand, that example is only *** eample, not Swiss clock. Tgfx tick is not valid timebase , technicaly crystal RTC need too special calibrating for one week precise clock ...

For real clock you rewrite example code ... Here dont work many design thinks, for example hours dont move between ...

Andrew Neil
Super User

Another one caught out by this:

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/massive-analog-digital-clock-time-delay-in-touchgfx-clock/m-p/763579

@mƎALLEm @Imen.D @Mohammad MORADI ESFAHANIASL - would be good to ensure the documentation makes this clear!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.