cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX 4.23.1 task doesn't close and remain open on multiple istances

matteo_lazzaro
Associate II

Hello,

the last release of TouchGFX has a problem when closed..

The problem is that when I close it, the task doesn't close and instead remain open.

See the attached image.

It appears to be open in multiple instances.

1 ACCEPTED SOLUTION

Accepted Solutions
Osman SOYKURT
ST Employee

Hello @matteo_lazzaro ,

This issue is resolved in the last TouchGFX release (4.23.2) available here : https://www.st.com/en/development-tools/touchgfxdesigner.html

I invite you to download and try that new version 

Osman SOYKURT
ST Software Developer | TouchGFX

View solution in original post

6 REPLIES 6
Osman SOYKURT
ST Employee

Hello @matteo_lazzaro ,

Thanks for reporting, could you give us more details please? Like does it happen every time or only with a specific project? Is your project heavy (lot of assets/screens/texts)? Which version of Windows do you use? Do you reproduce your issue on another computer? Do you reproduce it in an other version of TouchGFX?

We could analyze the logs if you send it to us. It's located under C:\Users\YOUR_USERNAME\AppData\Roaming\TouchGFX-4.23.1\TouchGFXDesigner.log

Osman SOYKURT
ST Software Developer | TouchGFX
matteo_lazzaro
Associate II

Hello Osman,

I have only one project to test and it happen always when I open it with TouchGFX 4.23.1.

My project is not so heavy, 26 screens but with many layers in it. Many texts.

I use Windows 10 Pro version 22H2.

My collegue with Windows 11 doesn't have this problem. Another my collegue with Windows 10 22H2 has the same problem.

Before, when i used TouchGFX 4.23.0 I didn't have this problem.

 

This is the log:

2024-02-06 15:04:23,606 [1] INFO TouchGFXDesigner.App: Logging configured
2024-02-06 15:04:31,790 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: matteo.lazzaro
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.23.1
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.23.1\designer
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19045.0
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: it-IT
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :
2024-02-06 15:04:31,791 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: /
2024-02-06 15:04:31,792 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.09037 Full 4.8.09037 ) v4.0 (Client 4.0.0.0 )
2024-02-06 15:05:55,338 [11] INFO TouchGFXPackages.Implementation.FileDownloader: Take operation was canceled. IsCancellationRequested=True
2024-02-06 15:05:55,366 [1] INFO TouchGFXDesigner.Main.MainWindow: Application closed

My collegue with the same problem has the same log.

So when the log says that TouchGFX is closed, it is not closed and keep more of 3GB of ram occupied.

Hello,

Could you send us the entire log file please? Also, if you could share the project it would help me to investigate (you can share me in private if you prefer).
Also, can you test with a new empty application and tell me if the issue happens? 

Osman SOYKURT
ST Software Developer | TouchGFX
Osman SOYKURT
ST Employee

Hello @matteo_lazzaro ,

I received the log file, we'll investigate and get back to you. Meanwhile, I invite you to work on 4.23.0 if the bug does not happen on that version. Or you can end the process in Windows Task Manager if you face it again on 4.23.1.

Osman SOYKURT
ST Software Developer | TouchGFX
matteo_lazzaro
Associate II

Okay, thank you.

Osman SOYKURT
ST Employee

Hello @matteo_lazzaro ,

This issue is resolved in the last TouchGFX release (4.23.2) available here : https://www.st.com/en/development-tools/touchgfxdesigner.html

I invite you to download and try that new version 

Osman SOYKURT
ST Software Developer | TouchGFX