cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX 4.17.0 ,"you are not connected to internet" error is showing

SV
Associate

Hi,

when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .

thanks and regards

sinduja

This discussion is locked. Please start a new topic to ask your question.
60 REPLIES 60

Thank you for the answer. I understand your current situation. I'll wait for your updating.

Current my situations are the follows:

4.16.1 : Proxy error occurs and proxy dialog appears repeateadly.

4.17.0 : Proxy error occurs but proxy dialog doesn't appears. I placed the file "STM32H735G-DK-3.0.5.tpa" which you provided in "C:\TouchGFX\4.17.0\app\packages\".

4.18.0 : Proxy error occurs and proxy dialog appears repeateadly. I placed the files "STM32G071-NUCLEO-DEMO-3.0.1.tpa" and "STM32G071-NUCLEO-DEMO-test-3.0.1.tpa" which you provided in "C:\TouchGFX\4.18.0\app\packages\".

So far I have to use only 4.17.0.

Resolved by myself. Proxy certification was changed. I modified it and works correctly.

I'm very sorry for your trouble.

Thank you.

JClar.7
Associate II

I'm running TouchGFX 4.18.0 and I also get the "You are not connected to the internet" error.

The TouchGFX Designer log shows: "System.Security.Authentication.AuthenticationException: Authentication failed because the remote party sent a TLS alert: 'HandshakeFailure'."

The error I've got appears to be with the server rejecting the connection, not my machine rejecting the certificate. So it's not the same proxy error, but is related to SSL on the server.

I'm running Win7, which supports up to TLS1.2. I tried installing on a Windows 10 laptop and it worked. Windows 8 and 8.1 also only have support for TLS up to 1.2.

I can access this image https://sw-center.st.com/touchgfx/pacman/4.17.0/STM32F746G_DISCO/STM32F746G-DISCO_front.png in FireFox, which uses it's own encryption library. If I try to access it in old Internet Explorer, I get the following error:

"This page can’t be displayed

Turn on TLS 1.0, TLS 1.1, and TLS 1.2 in Advanced settings and try connecting to https://sw-center.st.com again. If this error persists, it is possible that this site uses an unsupported protocol or cipher suite such as RC4 (link for the details), which is not considered secure. Please contact your site administrator. "

TLS 1.0, TLS 1.1, and TLS 1.2 are all turned on in IE advanced settings. Checking the connection when FireFox loads the page, it is using TLS 1.3

If TouchGFX Designer is relying on the OS for encryption, then in order to support the features on Windows 7 and 8, ST would need to enable TLS 1.2 on the server that TouchGFX connects to.

JPark.28
Associate II

Hi

I'm getting exactly the same problem as JClar.7. I only run Windows 7 and Linux so Win 10 is not an option for me.

Any suggestions on how to get TouchGFX working?

Are ST looking into this?

Many thanks

Kind regards

John

JClar.7
Associate II

I opened a ticket with ST. I got a reply last night that said:

"We have escalated your inquiry to our applications team for further support."

Hopefully they'll sort it out soon.

JPark.28
Associate II

Excellent - I look forward to seeing some progress

Kind regards

John

Hello,

any news about this issue?

Thanks.

LTyma.1
Associate

Hi,

I have the same problem. Running on win 7

Thanks

EMir.1
Associate II

Hi,

I have the same problem with touchGFX 4.17 , 4.18.0 and 4.18.1 with Win7.

Someone have solved this problem?

Thanks

Enal

JClar.7
Associate II

I got an answer to my support ticket. It looks like they're not going to fix it for Windows 7 users. I did repeatedly try to make it clear to them that the issue could be resolved by enabling TLS 1.2 on the server and did not actually require an update to the client app, but they never acknowledged those parts of my messages. Their response to the support ticket below:

"

I just got the final answer from the TouchGFX technical team :

"It was decided that we will not try to support Windows 7 or 8 for TouchGFX 4.17 and above.

The workaround would be to send them the .tpa for the boards they wish to work with and have them add it to the \TouchGFX\4.18.0\app\packages.

It is in our plan (for 4.19 maybe) to have a package to share will all the tbs, or an open git repo but it won't be in the near future."

I think this decision is not only based on TLS but also on internal circuitry of the Designer that relies on Windows SDL2 API.

Sorry for the inconvenience,

"