2020-04-16 12:51 PM
Hi,
I am struggling Struggling with TouchGFX Generated Code Building on STM32Cube IDE.
I am working on below setup:
Software Tool Chain:
STM32CubeMX 5.6.0
TouchGFX 4.13.0 Designer
STM32CubeIDE 1.3.0
Hardware:
STM32F746G-DISCO (Discovery Board)
I have created GUI on TouchGFX 4.13.0. worked fine on simulator and Discovery Board as well.
I am doing as below :
Open TouchGFX:
1. File->New
2. Select Application Template STM32F746G Discovery Kit
3. Select UI Template -> Blank UI
4. Name the project TestHardware and Click Create
5. Add a Red box that fills with rectangle and the entire canvas.
6. Add a button that I can click
7. Click Generate Code
8. Click Run Target
This does work, and I get the desired Red box and single button that I can click.
When I am trying to Open In STM32CubeIDE 1.3.0 and Import as per below:
C:\TouchGFXProjects\TestHardware\STM32CubeIDE
Binary File Created in Too Large ..
1) STM32F746G_DISCO.bin 2.12 GB
STM32F746G_DISCO.elf 239 KB
STM32F746G_DISCO.hex 99 KB
2) STM32CubeIDE Debugger Error !!
(Read) Failed determine breakpoint type
Error ! Failed to read target status
Debugger connection lost.
Shutting down . . .
3) STM32CubeProgrammer 2.4.0 also have Error while programming .But The TouchGFX Generated File works Well.
4) Changing the STM32F746NGHx_FLASH.ld (from Repository Demo of specific board ) reduce the file size to 35KB . But Code did not work on target either Debug Mode receive error at mention 2) nor the STM32CubeProgrammer/ST-Link.
Is this is Bug or I am using something wrong. ? Please advice me ..
Thanks in advance
--
Karan
Solved! Go to Solution.
2020-04-27 3:51 AM
No it's not a bug. It's normal. You shouldn't use the .bin file.
The only interesting files are .elf file and .hex file to download you project into your board.
You can remove the generation of the .bin file by unchecking the option in the project settings.
/Alexandre
2020-04-16 1:49 PM
You have to debug the *.elf, not the *.bin... There´s also the possibility to switch off the building of the *.bin files, if they´re not needed. (can´t take a closer look, where exactly to do so :( my laptop is not within reach right now... It was somewhere in Properties, c/c++ build...)
For now it should work to go to your debug configuration and choose the correct file (the *.elf) :)
2020-04-17 2:30 AM
Thanks for update ... But Still same result ..
(Read)Failed determine breakpoint type
Error! Failed to read target status
Debugger connection lost.
Shutting down...
Anybody from ST please Advice ?
2020-04-17 6:38 AM
Take a look at Project -> Properties -> Run/Debug Settings. In the right pane double click on your debug configuration. Tab "Main": Is the correct file set up there ? (Normally "Debug\<ProjectName>.elf")
2020-04-17 7:02 AM
Hello,
"When I am trying to Open In STM32CubeIDE 1.3.0 and Import as per below" -> What do you mean by You tried to import ?
"Changing the STM32F746NGHx_FLASH.ld" -> What sort of change did you do to the linker file ?
The steps you described are correctly done. And it's proven by the fact that it works using the Designer. So the issue comes to what you did right after to go to CubeIDE.
Normally, you just need to double-click on the .project in the STM32CubeIDE/ folder and build since you started from the AT.
/Alexandre
2020-04-17 9:52 AM
@chaaalyy (Community Member) Thanks .. Yes.. This is exactly same . But Still not working..
@Alexandre RENOUX (ST Employee)
Thanks you too .
I have tried to open .project as well .
Binary File Created in Too Large ..
STM32F746G_DISCO.bin 2.12 GB
STM32F746G_DISCO.elf 239 KB
STM32F746G_DISCO.hex 99 KB
2) STM32CubeIDE Debugger Error !!
(Read) Failed determine breakpoint type
Error ! Failed to read target status
Debugger connection lost.
Shutting down . . .
Then I have Just replaced linker file from
C:\Users\Abc\STM32Cube\Repository\STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\Display\LTDC_PicturesFromSDCard\SW4STM32\STM32746G-DISCOVERY
to
C:\TouchGFXProjects\MyApplication_11\STM32CubeIDE
Output After Changing linker file
STM32F746G_DISCO.bin 45Kb
STM32F746G_DISCO.elf 1682 KB
But Code not working in Debug/release mode as well.
Can you checked Internally ? What is issue/bug/mistake while compiling/running code on target?
--
Karan
2020-04-17 12:06 PM
Ok, at the moment it´s a little bit like fortune telling, what exactly happened at your side to give you that behaviour of your toolchain...
So i would recommend to restart from scratch (could be done within 10 minutes...). Take a look at this video:
https://www.youtube.com/watch?v=12KXreXaLp0
Be sure to follow the instructions carefully and slowly. When it comes to differences because you have a newer version of firmware package etc., just answer yes or "migrate" at that point. Be really sure, not to miss any of the points from the video !
Good Luck and i wish you success =)
Edit: In some cases, if it won´t build... Generate code within touchGFX designer again, afterwards do a right click on the project and choose "refresh", so it can recognize all of the generated files ;)
2020-04-18 6:38 AM
Thanks for Link ..
But This video ..
This is Just a trick to run TouchGFX 4.13.0 on STM32CubeIDE 1.3.0
It does not a relevant method (I think) .
There is definitely is Bug from STM32CubeIDE/STMC32Cube/TouchGFX Side while integration.
Any way, I have made document to
How_to_Configure_STM32F746_Discovery_TouchGFX_4.13.0_STM32CubeIDE_1.3.0 . . . .
Hope this may help others..
@Alexandre RENOUX (ST Employee)
Did you get some time to check at your end? with your team Martin KJELDSEN (ST Employee)
--
Karan
2020-04-18 8:12 AM
Nice to see a crippled project ... It may build, but anyway not run correctly. You missed TWO very important parts: QSPI setup in Linker Script and also MPU configuration. But as far, as i see, you are the expert here and i´m just a stupid enough to watch any videos ;)
Maybe next time i also should forget about that stuff. As long, as this video provides a method, doable for (nearly...) everybody, i´ll keep on watching and have a lot of respect for the people, who are providing them and share their knowledge ;)
btw: exceptionally i have to say, this time it´s not the fault of ST or the tGFX team...
I also did a complete integration and hardware setup manually (the hard way...). Just to learn, what´s going on below the surface... And i have to say, it´s no problem, if you know the settings, you have to provide. These generators are no fortune tellers about any hardware, somebody wants to get up and running
2020-04-20 1:25 AM
Hello,
To have the same setup and be on the same track in order to avoid unwanted steps that we would not be aware of, please follow these steps:
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.