2023-03-03 01:27 AM
When I flash some .bin the LCD doesen't work. It just display the a noise picture. With similar examples does work and with more advanced examples like the EmbeddedWizard it works too.
When does not work, every time display the same static image:
Solved! Go to Solution.
2023-03-10 08:35 AM
p.s. The BSP example shows the issue.
2023-03-10 08:49 AM
Hello @ACapo.1
I also tested BSP with LCD rev A03 and board D01
EDIT: LCD_DSI example tested with board RevD01 and RevD03
Could you please check the board revision (Under LCD)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-10 09:30 AM
D03 here
2023-03-10 09:31 AM
I tried the BSP example again after reattaching the display to see if it had magically been fixed but still same problem.
Could you please attach your elf or hex here and I will flash that.
2023-03-10 09:38 AM
Hi,
DO3 here.
Board was from Mouser, there is also another guy having issues which may be related, also from mouser: https://community.st.com/s/question/0D53W00002ASl3lSAD/stm32h747-discovery-blank
Could you please attach your BSP example elf here and I will flash it so we can double check it isn't a software tool problem.
2023-03-10 09:54 AM
Colourful junk like this is more likely the memory behind the LTDC/DSI
The geometry, timing and DSI look to be working
2023-03-10 10:12 AM
Would suggest attaching a known working .HEX file, would remove a lot of variables in identifying what's wrong.
2023-03-10 10:58 AM
I don't know what is happening here but I have made posts that are not here now.
The board is RevD03, Sarra can you attach your working BSP example elf or hex and I will flash it.
2023-03-10 11:27 AM
Interestingly if you look at the image in the first post and the image I posted the screen looks vey similar, look at the vertical "lines".
2023-03-10 11:53 AM
Yes, I have the same board. The only difference that I see is in the sticker with the QR code. In mine is A225301364