cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 STM32N6570-DK DMA2D Not working

Hamady
Senior

Hello,

I'm trying to use the LTDC peripheral with DMA2D to be able to send a image to the display without using the CPU

So first i used the example LTDC_Horizontal_Mirroring to have a working LCD . Compiling it i have the dolphin on my screen and flip horizontally.

Next step i used the same config as the project DMA2D_MemoryTo_Memory. So DMA2D in M2M, ARGB4444 in input /ouput alpha input at 0xFF and enable the interrupt (done in my LTDC_Horizontal_Mirroring project)(Also enable I and D cache for cortex M55).

After i used the same code for the dma in the M2M project , but when i use the debug tool or put the ouput buffer in my screen i have only 0.

I checked all register for DMA and the config and adress for in and out (DMA) correspond to the address of the buffer i gave to DMA.

Any ideas ?

Thanks.

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "dolphin_156x129_565.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define LAYER_SIZE_X				16
#define LAYER_SIZE_Y				32
#define LAYER_NB_BYTES_PER_PIXEL	2 /* because ARGB4444 format in input texture */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

DMA2D_HandleTypeDef hdma2d;

LTDC_HandleTypeDef hltdc;

/* USER CODE BEGIN PV */
__ALIGN_BEGIN uint32_t aBufferResult[(LAYER_SIZE_X * LAYER_SIZE_Y * LAYER_NB_BYTES_PER_PIXEL) / 4] __attribute__((aligned(16))) __NON_CACHEABLE = {0};

/* ARGB4444 input buffer 16bpp */
__ALIGN_BEGIN uint32_t aBufferInput[(LAYER_SIZE_X * LAYER_SIZE_Y * LAYER_NB_BYTES_PER_PIXEL) / 4] __attribute__((aligned(16)))  =
{0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203,
0xEFFFFFF2, 0xAB1FFFF0, 0x0504044E, 0x89ADCDEF, 0x15248722, 0x5201245E, 0x01025FDE, 0xFE010203} ;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_LTDC_Init(void);
static void MX_DMA2D_Init(void);
/* USER CODE BEGIN PFP */
void MPU_Config(void);
static void TransferError(DMA2D_HandleTypeDef* dma2dHandle);
static void TransferComplete(DMA2D_HandleTypeDef* dma2dHandle);
ErrorStatus Buffercmp(uint32_t* pBuffer1, uint32_t* pBuffer2, uint32_t BufferLength);
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */
	 MPU_Config();
  /* USER CODE END 1 */

  /* Enable the CPU Cache */

  /* Enable I-Cache---------------------------------------------------------*/
  SCB_EnableICache();

  /* Enable D-Cache---------------------------------------------------------*/
  SCB_EnableDCache();

  /* MCU Configuration--------------------------------------------------------*/
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_LTDC_Init();
  MX_DMA2D_Init();
  /* USER CODE BEGIN 2 */
  BSP_LED_Init(LED1);
  BSP_LED_Init(LED2);
  /* DMA2D Callbacks Configuration*/
  hdma2d.XferCpltCallback  = TransferComplete;
  hdma2d.XferErrorCallback = TransferError;
  /* Start DMA2D transfer*/
  if(HAL_DMA2D_Start_IT(&hdma2d,
                        (uint32_t)&aBufferInput,  /* Source memory buffer      */
                        (uint32_t)&aBufferResult, /* Destination memory buffer */
                        LAYER_SIZE_X,             /* Width of the 2D memory transfer in pixels */
                        LAYER_SIZE_Y)             /* Height of the 2D memory transfer in lines */
     != HAL_OK)
  {
    /* Initialization Error */
    Error_Handler();
  }

 /* Wait for the end of the transfer*/
  /*  Before starting a new transfer, you need to check the current state of
  the peripheral; if it is busy you need to wait for the end of current
  transfer before starting a new one.
  For simplicity reasons, this example is just waiting till the end of the
  transfer, but application may perform other tasks while transfer operation
  is ongoing. */
  while (HAL_DMA2D_GetState(&hdma2d) != HAL_DMA2D_STATE_READY)
  {
    HAL_Delay(100);

    BSP_LED_Off(LED1);

    /* Check transfer correctness*/
    if(Buffercmp(aBufferInput,
                 aBufferResult,
                 ((LAYER_SIZE_X * LAYER_SIZE_Y * LAYER_NB_BYTES_PER_PIXEL) / 4)) == ERROR)
    {
      /* KO */
      /* Turn LD3 On */
      BSP_LED_On(LED2);
    }
    else
    {
      /* OK */
      /* Turn on LD1 */
      BSP_LED_On(LED1);
    }
  }

  HAL_LTDC_SetAddress(&hltdc, (uint32_t) dolphin_156x129_565, 0);
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
    HAL_Delay(1000);
    HAL_LTDC_ConfigMirror(&hltdc,LTDC_MIRROR_HORIZONTAL, 0);
    HAL_Delay(1000);
    HAL_LTDC_ConfigMirror(&hltdc,LTDC_MIRROR_NONE, 0);

  }
  /* USER CODE END 3 */
}
/* USER CODE BEGIN CLK 1 */

/*         The system Clock is configured as follows :
              CPU Clock source               = IC1_CK
              System bus Clock source        = IC2_IC6_IC11_CK
              CPUCLK (sysa_ck) (Hz)          = 600000000
              SYSCLK AXI (sysb_ck) (Hz)      = 400000000
              SYSCLK NPU (sysc_ck) (Hz)      = 300000000
              SYSCLK AXISRAM3/4/5/6 (sysd_ck) (Hz) = 400000000
              HCLKx(Hz)                      = 200000000
              PCLKx(Hz)                      = 200000000
              AHB Prescaler                  = 2
              APB1 Prescaler                 = 1
              APB2 Prescaler                 = 1
              APB4 Prescaler                 = 1
              APB5 Prescaler                 = 1
              PLL1 State                     = ON
              PLL1 clock source              = HSI
              PLL1 M                         = 4
              PLL1 N                         = 75
              PLL1 P1                        = 1
              PLL1 P2                        = 1
              PLL1 FRACN                     = 0
              PLL2 State                     = BYPASS
              PLL2 clock source              = HSI
              PLL3 State                     = BYPASS
              PLL3 clock source              = HSI
              PLL4 State                     = BYPASS
              PLL4 clock source              = HSI
*/
/* USER CODE END CLK 1 */

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the System Power Supply
  */
  if (HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY) != HAL_OK)
  {
    Error_Handler();
  }

  /* Enable HSI */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Get current CPU/System buses clocks configuration and if necessary switch
 to intermediate HSI clock to ensure target clock can be set
  */
  HAL_RCC_GetClockConfig(&RCC_ClkInitStruct);
  if ((RCC_ClkInitStruct.CPUCLKSource == RCC_CPUCLKSOURCE_IC1) ||
     (RCC_ClkInitStruct.SYSCLKSource == RCC_SYSCLKSOURCE_IC2_IC6_IC11))
  {
    RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_CPUCLK | RCC_CLOCKTYPE_SYSCLK);
    RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_HSI;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
    {
      /* Initialization Error */
      Error_Handler();
    }
  }

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_NONE;
  RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL1.PLLM = 4;
  RCC_OscInitStruct.PLL1.PLLN = 75;
  RCC_OscInitStruct.PLL1.PLLFractional = 0;
  RCC_OscInitStruct.PLL1.PLLP1 = 1;
  RCC_OscInitStruct.PLL1.PLLP2 = 1;
  RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL4.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL4.PLLM = 1;
  RCC_OscInitStruct.PLL4.PLLN = 25;
  RCC_OscInitStruct.PLL4.PLLFractional = 0;
  RCC_OscInitStruct.PLL4.PLLP1 = 1;
  RCC_OscInitStruct.PLL4.PLLP2 = 1;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_CPUCLK|RCC_CLOCKTYPE_HCLK
                              |RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
                              |RCC_CLOCKTYPE_PCLK2|RCC_CLOCKTYPE_PCLK5
                              |RCC_CLOCKTYPE_PCLK4;
  RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_IC1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_IC2_IC6_IC11;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
  RCC_ClkInitStruct.APB5CLKDivider = RCC_APB5_DIV1;
  RCC_ClkInitStruct.IC1Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC1Selection.ClockDivider = 2;
  RCC_ClkInitStruct.IC2Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC2Selection.ClockDivider = 3;
  RCC_ClkInitStruct.IC6Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC6Selection.ClockDivider = 4;
  RCC_ClkInitStruct.IC11Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC11Selection.ClockDivider = 3;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief DMA2D Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_DMA2D_Init(void)
{

  /* USER CODE BEGIN DMA2D_Init 0 */

  /* USER CODE END DMA2D_Init 0 */

  /* USER CODE BEGIN DMA2D_Init 1 */

  /* USER CODE END DMA2D_Init 1 */
  hdma2d.Instance = DMA2D;
  hdma2d.Init.Mode = DMA2D_M2M;
  hdma2d.Init.ColorMode = DMA2D_OUTPUT_ARGB4444;
  hdma2d.Init.OutputOffset = 0;
  hdma2d.LayerCfg[1].InputOffset = 0;
  hdma2d.LayerCfg[1].InputColorMode = DMA2D_INPUT_ARGB4444;
  hdma2d.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
  hdma2d.LayerCfg[1].InputAlpha = 255;
  if (HAL_DMA2D_Init(&hdma2d) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_DMA2D_ConfigLayer(&hdma2d, 1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN DMA2D_Init 2 */

  /* USER CODE END DMA2D_Init 2 */

}

/**
  * @brief LTDC Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_LTDC_Init(void)
{

  /* USER CODE BEGIN LTDC_Init 0 */

  /* USER CODE END LTDC_Init 0 */

  LTDC_LayerCfgTypeDef pLayerCfg = {0};

  /* USER CODE BEGIN LTDC_Init 1 */

  /* USER CODE END LTDC_Init 1 */
  hltdc.Instance = LTDC;
  hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
  hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
  hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
  hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
  hltdc.Init.HorizontalSync = 4;
  hltdc.Init.VerticalSync = 4;
  hltdc.Init.AccumulatedHBP = 12;
  hltdc.Init.AccumulatedVBP = 12;
  hltdc.Init.AccumulatedActiveW = 812;
  hltdc.Init.AccumulatedActiveH = 492;
  hltdc.Init.TotalWidth = 820;
  hltdc.Init.TotalHeigh = 500;
  hltdc.Init.Backcolor.Blue = 0;
  hltdc.Init.Backcolor.Green = 0;
  hltdc.Init.Backcolor.Red = 0;
  if (HAL_LTDC_Init(&hltdc) != HAL_OK)
  {
    Error_Handler();
  }
  pLayerCfg.WindowX0 = 0;
  pLayerCfg.WindowX1 = 156;
  pLayerCfg.WindowY0 = 0;
  pLayerCfg.WindowY1 = 129;
  pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB565;
  pLayerCfg.Alpha = 255;
  pLayerCfg.Alpha0 = 0;
  pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
  pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
  pLayerCfg.FBStartAdress = 0;
  pLayerCfg.ImageWidth = 156;
  pLayerCfg.ImageHeight = 129;
  pLayerCfg.Backcolor.Blue = 255;
  pLayerCfg.Backcolor.Green = 0;
  pLayerCfg.Backcolor.Red = 0;
  if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN LTDC_Init 2 */
    RIMC_MasterConfig_t RIMC_master = {0};
    RIMC_master.MasterCID = RIF_CID_1;
    RIMC_master.SecPriv = RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV;
    HAL_RIF_RIMC_ConfigMasterAttributes(RIF_MASTER_INDEX_LTDC1 , &RIMC_master);

    HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_LTDCL1 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV);
  /* USER CODE END LTDC_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  /* USER CODE BEGIN MX_GPIO_Init_1 */
  /* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOQ_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOE_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOQ, LCD_BL_CTRL_Pin|LCD_ONOFF_Pin, GPIO_PIN_SET);

  /*Configure GPIO pins : LCD_BL_CTRL_Pin LCD_ONOFF_Pin */
  GPIO_InitStruct.Pin = LCD_BL_CTRL_Pin|LCD_ONOFF_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOQ, &GPIO_InitStruct);

  /* USER CODE BEGIN MX_GPIO_Init_2 */
  /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void MPU_Config(void)
{
  MPU_Region_InitTypeDef default_config = {0};
  MPU_Attributes_InitTypeDef attr_config = {0};
  uint32_t primask_bit = __get_PRIMASK();

  /* disable the MPU */
  HAL_MPU_Disable();
  /* create an attribute configuration for the MPU */
  attr_config.Attributes = INNER_OUTER(MPU_NOT_CACHEABLE);
  attr_config.Number = MPU_ATTRIBUTES_NUMBER0;
  HAL_MPU_ConfigMemoryAttributes(&attr_config);
  /* Create a non cacheable region */
  /*Normal memory type, code execution allowed */
  default_config.Enable = MPU_REGION_ENABLE;
  default_config.Number = MPU_REGION_NUMBER0;
  default_config.BaseAddress = __NON_CACHEABLE_SECTION_BEGIN;
  default_config.LimitAddress =__NON_CACHEABLE_SECTION_END;
  default_config.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
  default_config.AccessPermission = MPU_REGION_ALL_RW;
  default_config.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
  default_config.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
  HAL_MPU_ConfigRegion(&default_config);

  /* enable the MPU */
  HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
  /* Exit critical section to lock the system and avoid any issue around MPU mechanisme */
  __set_PRIMASK(primask_bit);
}

/**
* @brief  DMA2D Transfer completed callback
* @PAram  hdma2d: DMA2D handle.
* @note   This example shows a simple way to report end of DMA2D transfer, and
*         you can add your own implementation.
* @retval None
*/
static void TransferComplete(DMA2D_HandleTypeDef *hdma2d)
{
  BSP_LED_On(LED1);
}

/**
* @brief  DMA2D error callbacks
* @PAram  hdma2d: DMA2D handle
* @note   This example shows a simple way to report DMA2D transfer error, and you can
*         add your own implementation.
* @retval None
*/
static void TransferError(DMA2D_HandleTypeDef *hdma2d)
{
  /* Turn LED red on  On */
  BSP_LED_On(LED2);
}
/**
* @brief  Compares two buffers.
* @PAram  pBuffer1, pBuffer2: buffers to be compared.
* @PAram  BufferLength: buffer's length.
* @retval  0: pBuffer1 identical to pBuffer2
*          1: pBuffer1 differs from pBuffer2
*/
ErrorStatus Buffercmp(uint32_t* pBuffer1, uint32_t* pBuffer2, uint32_t BufferLength)
{
  while (BufferLength--)
  {
    if (*pBuffer1 != *pBuffer2)
    {
      return ERROR;
    }
    pBuffer1++;
    pBuffer2++;
  }
  return SUCCESS;
}
/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */

   /* Turn On the Red Led */
   BSP_LED_On(LED2);

  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

1 REPLY 1
Hamady
Senior

Hamady_0-1743185880196.png

For info here all registers