2020-10-17 11:29 AM
Hi
Why doesn't releasing the offon button exits the loop until Job () is finished?
greetings
Andrzej
2020-10-23 6:27 AM
Hi, can you be a bit more specific? Is this your own project? What's supposed to happen and what doesn't happen? etc! Thanks!
/Martin
2020-10-23 7:45 AM
Hello
Yes, this is my own project.
I have a Toggle button "offon" on my desktop
The button status is in the message "messageQ4" to the "StartSecondTask" funcjon.
If offon = 1, Job () is to be called; The function is called. When I press the "offon" button it should be set to offon = 0; but it is not.
greetings
Andrzej
2020-10-28 11:36 PM
hello friend
Touchgfx does not work for me, I get the pixelated screen I use stm32cubeide 1.4.0 it does not work for me download version 1.2.0 and also download TouchGFX V4.14 and nothing, change the version ==> V4.13 and still some help friend , I hope you can help me ??
I made a simple program in touchgfx and there it works, but the detail is that I use LWIP in my program, I need to use it from stm32cubeide
2020-10-28 11:53 PM
I get the pixelated screen
2020-10-29 12:19 AM
hello friend
Touchgfx does not work for me, I get the pixelated screen I use stm32cubeide 1.4.0 it does not work for me download version 1.2.0 and also download TouchGFX V4.14 and nothing, change the version ==> V4.13 and still some help friend , I hope you can help me ??
I made a simple program in touchgfx and there it works, but the detail is that I use LWIP in my program, I need to use it from stm32cubeide