2020-04-21 8:26 AM
Hi!
I set CubeIDE as in the tutorial https://www.youtube.com/watch?v=12KXreXaLp0&t=3s
I set FreeRTOS.
In main.c I have
void secondTask (void const * argument) {
for (;;) {
xQueueSend (messageQ1, & poster, 0);
osDelay (1);
}
}
The program runs to this function but stops there.
Why?
I'm sending Model.cpp
Andrzej
2020-04-21 9:20 AM
2020-04-21 10:31 AM
Hi =) If you follow the steps from the video, everything should be fine. Does it run, if you comment out the "xQueueSend..." ? Anyway: You send the Message far more often, than you can handle it... You send every 1ms (more or less) and in model::tick() usually gets called with 60Hz ... I´m not used to XQueue, but i don´t see any external declaration of "poster" in model.cpp ...
2020-04-22 5:00 AM
Hi!
I changed the time but it did nothing.
The ( uint8_t poster ) declaration is in the Model.hpp file. Is that enough
Earlier I uncommented xQueueSend the program did not crash.
Now the program compiles without errors but there is a bad picture.
I have to start again. I'll write if I manage.
Thank you
Andrew
2020-04-22 5:01 AM
Thank you!
I will check and answer
Andrzej
2020-04-22 7:08 AM
No work.
error:
/STM32TouchController.o"
../TouchGFX/target/generated/OSWrappers.cpp:17:10: fatal error: touchgfx/hal/OSWrappers.hpp: No such file or directory
#include <touchgfx/hal/OSWrappers.hpp>
^~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
In file included from ../TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp:18:0:
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp:20:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory
#include <touchgfx/hal/HAL.hpp>
^~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [TouchGFX/target/generated/subdir.mk:27: TouchGFX/target/generated/OSWrappers.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [TouchGFX/target/generated/subdir.mk:33: TouchGFX/target/generated/TouchGFXGeneratedHAL.o] Error 1
../TouchGFX/target/generated/TouchGFXConfiguration.cpp:17:10: fatal error: texts/TypedTextDatabase.hpp: No such file or directory
#include <texts/TypedTextDatabase.hpp>
^~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
In file included from ../TouchGFX/target/STM32TouchController.cpp:20:0:
../TouchGFX/target/STM32TouchController.hpp:22:10: fatal error: platform/driver/touch/TouchController.hpp: No such file or directory
#include <platform/driver/touch/TouchController.hpp>
^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [TouchGFX/target/generated/subdir.mk:31: TouchGFX/target/generated/TouchGFXConfiguration.o] Error 1
make: *** [TouchGFX/target/subdir.mk:24: TouchGFX/target/STM32TouchController.o] Error 1
../TouchGFX/target/generated/STM32DMA.cpp:20:10: fatal error: touchgfx/hal/OSWrappers.hpp: No such file or directory
#include <touchgfx/hal/OSWrappers.hpp>
^~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [TouchGFX/target/generated/subdir.mk:29: TouchGFX/target/generated/STM32DMA.o] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
15:59:13 Build Failed. 11 errors, 0 warnings. (took 3s.995ms)
2020-04-22 7:26 AM
Sounds to me like your include path is not pointing correctly to touchgfx :) Show your include path settings
/Martin