2022-11-08 10:40 PM
Hi, I initialized 2 layers in LTDC to show 2 images, which was done directly by addressing them from flash.
That was fine till I want to set 2 layers in my SDRAM.
application note has said the first one should be addressed in 0xc0000000 and the second one should be configured in a bank addition to first layer.
The problem is 2 layers independently work but to enable them at the same time, they won't work properly.
Have some one faced with this problem?
what should I do to enable them at the same time?
stm 32f429
LTDC is configured in 16 bits.
2022-11-09 06:59 AM
Why you need two layers in ram?
Is layers too RGB565 ?
How dotclock you use for LTDC? ...
show layer2 addr too. for check.
What is wont work prop...
2022-11-20 11:16 PM
Hi, sorry for my late reply, I didn't understand what dotclock in LTDC is.
I finally set 2 layers in SDRAM but, I got some tempering with images I thought that was due to my SDRAM configuration.
I meant it is possible to address directly your buffers which can be images... in SDRAM, but you should know to address them n 2 different SDRAM banks.
Now, I have another question:
I am using TOUCHGFX, in my project I have to display 12 graphs in two columns (2*6), I want to have grids behind my graphs for this case I don't use minor and major grid lines for graphs, I wrote them manually by lines....
when I use vertical frontline for my dynamic graph, the line erase my behind grids too.
Is there any idea to help me frontline doesn't erase the behind grids?