‎2021-03-20 12:04 PM
I set up TouchGFX:
https://www.youtube.com/watch?v=9QDWti5RzBU
I have: STM32CubeIDE 1.6.0, TouchGFX 4.16.1
warning:
Description Resource Path Location Type
Invalid project path: Include path not found (C:\Users\ad\STM32CubeIDE\workspace_1.6.0\testad_1\Middlewares\Third_Party\FreeRTOS\Source\CMSIS_RTOS). testad_1 pathentry Path Entry Problem
Works fine, but I can't move from CubeIDE to GFX. why?
Andrzej
Solved! Go to Solution.
‎2021-03-23 05:36 AM
Hi,
The video was a good idea but I cannot read polish so it is quite complicated to understand the context of it and what you are trying to do. Could you give us more detail through writing ?
/Romain
‎2021-03-22 03:29 AM
Hi,
Try changing the workspace to somewhere directly in C (or C:\tempoWorkspace or something).
/Romain
‎2021-03-22 03:30 AM
I would also advise to edit the tag section to add "STM32CubeIDE" to increase the visibility of your post.
/Romain
‎2021-03-22 12:03 PM
Hi
Does not help.
Andrzej
‎2021-03-22 11:05 PM
Hi,
Saying "does not help" will not make you find an answer more quickly.
What do you mean by you cannot move from CubeIDE to GFX.
What are the steps you did ? Did you create your project from scratch using CubeIDE ? Or started with the Application Template available in the Designer? The latter is highly recommended.
/Alexandre
‎2021-03-23 03:00 AM
Hi
aying "does not help" will not make you find an answer more quickly.
What do you mean by you cannot move from CubeIDE to GFX.
What are the steps you did ? Did you create your project from scratch using CubeIDE ? Or started with the Application Template available in the Designer? The latter is highly recommended.
Andrzej
‎2021-03-23 05:36 AM
Hi,
The video was a good idea but I cannot read polish so it is quite complicated to understand the context of it and what you are trying to do. Could you give us more detail through writing ?
/Romain
‎2021-03-23 11:21 AM
Hi
I went back to the way I had used so far. He's not a problem.
https://www.youtube.com/watch?v=12KXreXaLp0&t=3s
Andrzej
‎2021-03-24 12:24 AM
Well good to hear that you are still able to work 😅
/Romain
‎2021-03-24 02:18 AM
Hi
Maybe I'm wrong but it seems to me that GFX sets IDE parameters and when I change them in the IDE an error is generated. The second disadvantage is the lack of a tab with switching to GFX in IDE / Project Explorer / ....
Andrzej