‎2022-04-23 5:04 PM
Hi,
I have three projects, running on an STM32H7B3I-DK Discovery board.
They Are:
Complex - Using TouchGFX, a lot of I/O, timers, ADC's I2C, SPI and the other project is simple using only the ADC's. Throws SWV error
Simple - No TouchGFX using ADC 1 and ADC 2 Only No SWV Error
Simple - Using Touch GFX and no other I/O No SWV Error
When I debug the complex project I get an error: "Failed To Enable SWI - SWV will be disabled for this debug session" When I debug the simple project the error does not occur.
Obviously it is something in the build of the complex project that is causing this. The debug settings are identical for each project and are shown in the screen shots attached.
The console output for the debug build is:
STMicroelectronics ST-LINK GDB server. Version 6.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 31
Listen Port Number : 651234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
COM frequency = 24000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fefd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V3J9M3
Device ID: 0x480
PC: 0x8000bb4
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.27 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Stm32Device, pollAndNotify running...
SwvSrv state change: 0 -> 1
Waiting for connection on port 61412...
Waiting for debugger connection...
Waiting for connection on port 61410...
Accepted connection on port 61410...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61410...
GDB session thread running
GdbSessionManager, session started: 1
Accepted connection on port 61410...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61410...
GDB session thread running
GdbSessionManager, session started: 2
Stm32Device, closeDevice() entry
GDB session, device event: 5
GDB session, device event: 5
Stm32Device, pollAndNotify stopped
Stm32Device, closeDevice() exit
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.10.0
-------------------------------------------------------------------
Log output file: c:\users\admin\appdata\local\temp\stm32cubeprogrammer_a35960.log
ST-LINK SN : 002D00483438511534313939
ST-LINK FW : V3J9M3
Board : STM32H7B3I-DK
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x480
Revision ID : Rev Z
Device name : STM32H7A/B
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
Memory Programming ...
Opening and parsing file: st-link_gdb_server_a35960.srec
File : st-link_gdb_server_a35960.srec
Size : 212.70 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 25]
Erasing memory corresponding to segment 1:
Erasing external memory sector 0
Download in Progress:
�������������������������������������������������� 0%
�������������������������������������������������� 100%
File download complete
Time elapsed during download operation: 00:00:00.804
Verifying ...
Read progress:
�������������������������������������������������� 50%
� 2%� 4%� 6%� 8%� 10%� 12%� 14%� 16%� 18%� 20%� 22%� 24%� 26%� 28%� 30%� 32%� 34%� 36%� 38%� 40%� 42%� 44%� 46%� 48%� 50%� 52%� 54%� 56%� 58%� 60%� 62%� 64%� 66%� 68%� 70%� 72%� 74%� 76%� 78%� 80%� 82%� 84%� 86%� 88%� 90%� 92%� 94%� 96%� 98%� 100%
Download verified successfully
------ Switching context -----
COM frequency = 24000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fefd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V3J9M3
Device ID: 0x480
PC: 0x8000bb4
ST-LINK detects target voltage = 3.30 V
ST-LINK device status: HALT_MODE
GDB session, device event: 6
GDB session, device event: 6
Stm32Device, pollAndNotify running...
GDB session, device event: 3
GDB session, device event: 3
GDB session, device event: 1
GDB session, device event: 1
GDB session, device event: 0
GDB session, device event: 0
NVIC_DFSR_REG = 0x0000000B
The debug console output is:
GNU gdb (GNU Tools for STM32 10.3-2021.10.20211105-1100) 10.2.90.20210621-git
Copyright (C) 2021 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.
Type "show copying" and "show warranty" for details.
This GDB was configured as "--host=x86_64-w64-mingw32 --target=arm-none-eabi".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<https://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
<http://www.gnu.org/software/gdb/documentation/>.
For help, type "help".
Type "apropos word" to search for commands related to "word".
Warning: the current language does not match this frame.
set *(int *)0xE000EDFC=*(int *)0xE000EDFC|0x7F0
set *(unsigned int *)0x5c001004|=0x3f
Temporary breakpoint 3, main () at G:/ShorttClock_V2/ShorttClock_V2/Core/Src/main.c:124
124 MPU_Config();
I turned logging on in the debug config, but it didn't produce the file listed in the console output:
c:\users\admin\appdata\local\temp\stm32cubeprogrammer_a35960.log
There was a file called LWSDebugOut.txt created at the same time as the debug session. It was 11 MByte and too large to attach.
I have the following questions:
Any ideas on what might be the problem?
best regards
Rob
Solved! Go to Solution.
‎2022-04-26 1:03 AM
Hello there,
I believe the problem might be in the port number. In the STM32H7B3I_DISCO project the port number 651234 is used instead of the default 61234 which makes the port number way too big.
‎2022-04-26 1:03 AM
Hello there,
I believe the problem might be in the port number. In the STM32H7B3I_DISCO project the port number 651234 is used instead of the default 61234 which makes the port number way too big.
‎2022-04-26 8:44 PM
Hi Markus,
Yep! You are right.
I must have had another senior's moment.
I had a support ticket on this, could you close it for me please.
Sorry to waste your time on silly mistakes.
Thanks
Rob
‎2022-04-27 1:54 AM
Hello Rob,
Those tickets are not managed at my level so unfortunately I can't close it for you. If you communicate through the OLS interface and mention that it's solved I'm sure they'll be happy to have an "open-and-shut" case ;)
Also, even if it was an easy mistake to correct this time the amount of information coupled with the screenshots always makes these things easier to analyze, so thank you for that. Happy to help!
‎2022-04-27 7:16 PM
Hi Markus,
I will put a comment through the OLS.
I always try to provide as much info as I can. In fact framing the question is often much harder than the solution. I have put together complicated questions a number of times then, because you have to go through a logical process to do this you actaully come up with the answer without actually having to post the question.
best regards
Rob