cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE Middleware > Graphics not available when using STM32F746G-Disco board

Rajssss
Associate II

I am using STM32CUBE IDE v1.6.0 with TouchGFX v4.16.1 installed and using firmware version V1.16.0.

Yet in the Middleware sections, the graphics section is not there.

Can anyone tell me why? 0693W000008y4wkQAA.jpg0693W000008y4wQQAQ.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

You skip one step, add pack to project and in new version you see it under midleware not in.

On your first image click on second line TouchGFX expand and add...

View solution in original post

2 REPLIES 2
MM..1
Chief III

You skip one step, add pack to project and in new version you see it under midleware not in.

On your first image click on second line TouchGFX expand and add...

Thanks, this worked.