2019-07-16 06:38 AM
Hi, I am trying to create a project in CubeMX for the TrueStudio but i can not connect the round LCD(MB1314). I am using the STM32L4R9I-Eval
I already tried to use the application examples present in the Repository but I only connect to an image through DSI, but with STemWin the screen never turns on.
I need help with some example or if possible with the *.ioc file.
Thanks.
2019-07-23 05:44 AM
Hi, there is an Hello World example at 'STM32 Repository\STM32Cube_FW_L4_V1.14.0\Projects\STM32L4R9I-EVAL\Applications\STemWin\MB1314\HelloWorld'. I hope this helps.