2019-06-28 2:27 AM
Hello,
i tried to get the STM32F446ZE and the STemWin Library running in a Keil Project.
The used OS is emOS from Segger.
I tried to follow you instructions to display "hello world" on the display.
I use the display driver ST7735S which should be supported by the FlexColor driver.
My problem is that instead of "hello world" the display stays white.
I configured GUIConf.h like that
#define GUI_NUMBYTES 0x8000In GUI_x I added the following in GUI_X_init() :
void GUI_X_Init(void) {
UC_ST7735_init();
USInt current = Sopas_usiGet_IOLink14360ST7735DisplayBacklightCurrent();
LITA_setDisplayCurrent((uint8_t)current);
}
In UC_ST7735_init() the SPI-Port gets intiated. This part should work because it ist already used in the same sensor type. The only difference is, that I removed the graphcis library we used before. The addition lines activate the display and it's backlight.
In LCDConf_FlexColor_Template.c I set the resolution like this:
#define XSIZE_PHYS 100 // To be adapted to x-screen size
#define YSIZE_PHYS 40 // To be adapted to y-screen sizeI filled the following three methods like that:
(It should be metioned that UC_ST7735_writeSPI4Wire was also used before and should work. It sends one byte after each other instead of 16 bit at once.
I tried to send the high byte and the low byte in different orders.)
static void LcdWriteReg(U16 Data) {
uint8_t data[2];
UC_ST7735_dcFLAG_t dcFlag = UC_ST7735_COMMAND;
data[0] = (uint8_t)UTIL_HLP_LOW_BYTE_OF_INT16(Data);
data[1] = (uint8_t)UTIL_HLP_HIGH_BYTE_OF_INT16(Data);
UC_ST7735_writeSPI4Wire(&data[1], 1, dcFlag);
UC_ST7735_writeSPI4Wire(&data[0], 1, dcFlag);
}
static void LcdWriteData(U16 Data) {
UC_ST7735_dcFLAG_t dcFlag = UC_ST7735_DATA;
uint8_t data[2];
data[0] = (uint8_t)UTIL_HLP_LOW_BYTE_OF_INT16(Data);
data[1] = (uint8_t)UTIL_HLP_HIGH_BYTE_OF_INT16(Data);
UC_ST7735_writeSPI4Wire(&data[1], 1, dcFlag);
UC_ST7735_writeSPI4Wire(&data[0], 1, dcFlag);
}
static void LcdWriteDataMultiple(U16 * pData, int NumItems) {
UC_ST7735_dcFLAG_t dcFlag = UC_ST7735_DATA;
uint8_t data[2];
int start_size = NumItems;
while (NumItems--) {
data[0] = (uint8_t)UTIL_HLP_LOW_BYTE_OF_INT16(pData[start_size-NumItems]);
data[1] = (uint8_t)UTIL_HLP_HIGH_BYTE_OF_INT16(pData[start_size-NumItems]);
UC_ST7735_writeSPI4Wire(&data[1], 1, dcFlag);
UC_ST7735_writeSPI4Wire(&data[0], 1, dcFlag);
}
}I didn't change the LCD_X_config for the Flexcolor driver
void LCD_X_Config(void) {
GUI_DEVICE * pDevice;
CONFIG_FLEXCOLOR Config = {0};
GUI_PORT_API PortAPI = {0};
//
// Set display driver and color conversion
//
pDevice = GUI_DEVICE_CreateAndLink(GUIDRV_FLEXCOLOR, GUICC_565, 0, 0);
//
// Display driver configuration, required for Lin-driver
//
LCD_SetSizeEx (0, XSIZE_PHYS , YSIZE_PHYS);
LCD_SetVSizeEx(0, VXSIZE_PHYS, VYSIZE_PHYS);
//
// Orientation
//
Config.Orientation = GUI_SWAP_XY | GUI_MIRROR_Y;
GUIDRV_FlexColor_Config(pDevice, &Config);
//
// Set controller and operation mode
//
PortAPI.pfWrite16_A0 = LcdWriteReg;
PortAPI.pfWrite16_A1 = LcdWriteData;
PortAPI.pfWriteM16_A1 = LcdWriteDataMultiple;
PortAPI.pfReadM16_A1 = LcdReadDataMultiple;
GUIDRV_FlexColor_SetFunc(pDevice, &PortAPI, GUIDRV_FLEXCOLOR_F66708, GUIDRV_FLEXCOLOR_M16C0B16);
}The code I run is:
GUI_Init();
int xPos, yPos;
//__HAL_RCC_CRC_CLK_ENABLE();
xPos = LCD_GetXSize() / 2;
yPos = LCD_GetYSize() / 3;
GUI_SetFont(GUI_FONT_COMIC24B_ASCII);
GUI_DispStringHCenterAt("Hello world!", xPos, yPos);
// Endless loop:
while(true)
{
OS_TASK_Delay(100);
MW_TWD_arm(); // Arm the watchdog
}There is no Compile-Error and the Watch Dog does not cause a problem.
The problem is that the display stays white.
I noticed that the command number which the flexchain driver sends over spi does not match the excpeted numbers from the St7735 datasheet.
I debugged the SPI method. The follwing commands and data got sent.
- a command with 0x00 as the high byte
- a command with 0x03 as the low byte. As far I know there is no command number 3 for theSTt7735
- data with 0x00 as the high byte
- data with 0x00 as the low byte
- a command with 0x00 as the high byte
- a command with 0x50 ('P') as the low byte.
- data with 0x00 as the high byte
- data with 0x00 as the low byte
- a command with 0x00 as the high byte
- a command with 0x51 ('Q') as the low byte.
- data with 0x00 as the high byte
- data with 0x63 as the low byte
- a command with 0x00 as the high byte
- a command with 0x52 as the low byte.
- data with 0x00 as the high byte
- data with 0x00 as the low byte
...
- after a while with more alternating commands and data there is just data with 0x00
Did I forget to config something?
Mit freundlichen Grüßen / Best regards
Lukas Hauser
2019-07-01 1:20 AM
Changing GUIDRV_FLEXCOLOR_F66708 to GUIDRV_FLEXCOLOR_F667089 helped in order to get the right command numbers for the ST7735 display driver.
Changing GUIDRV_FLEXCOLOR_M16C0B16 to GUIDRV_FLEXCOLOR_M16C1B8 doesn't. My device reboots before any SPI communication happens.
I debugged the program to known when The error occurs.
I runs the following methods without crashing but after the last one I didn't see an other name of a method in the disassmbly window of Keil.
emwin_LCD_init
LCD_SETBk_ColorIndex
LCD_set_ClipRectMax
GUI_Alloc_getFixedBlock
GUI_Device_GetpDriver
GUIDRV_Flexcolor_InitOnce
GUI_Alloc_getFixedBlock
LCD_X_DisplayDriver
It get's to the end of LCD_X_DisplayDriver but never to LcdWriteReg, LcdWriteData, LcdWriteDataMultiple or LcdReadDataMultiple.
What could be the problem? It's hard to debug without having the code.
2019-07-23 1:00 AM
Changing the default to this solved my problem:
// Set controller and operation mode
//
PortAPI.pfWrite8_A0 = LcdWriteReg;
PortAPI.pfWrite8_A1 = LcdWriteData;
PortAPI.pfWriteM8_A1 = LcdWriteDataMultiple;
// PortAPI.pfRead8_A1 = LcdReadData;
// PortAPI.pfReadM8_A1 = LcdReadDataMultiple;