cancel
Showing results for 
Search instead for 
Did you mean: 

ST32L4R9I-DISCO Demo Code

Christoph1
Associate II

Hello,

I would like to use a lot from the ST32L4R9I-DISCO Demo Code for my own application.

Are you planning to release the source code?

Thanks and best regards,

Christoph

1 ACCEPTED SOLUTION

Accepted Solutions
Martin KJELDSEN
Chief III

Hi guys,

Please find attached the l4r9-disco TouchGFX demo.

View solution in original post

7 REPLIES 7
Uwe Bonnes
Principal III

Do you mean Disco or Nucleo or Eval. Only a Eval board is found on the website. Did you check

STM32Cube/Repository/STM32Cube_FW_L4_V1.13.0/Projects/STM32L4R9I-EVAL/Examples/?

Martin KJELDSEN
Chief III

Hi @Christoph​,

I'm pretty sure the source code for the demo in question is not a part of the Cube firmware pack. I will check to see if i can make it available.

Best regards,

Martin

Hi @Martin KJELDSEN​

I have checked all available Code but the TouchGFX demo for ST32L4R9I-DISCO was only available as binary :sad_but_relieved_face: .

Thanks, that would be very nice =) and I think also other developers would appreciate it.

Best regards,

Christoph

Yes, I would love to take a look at the source code to determine some of the features to implement as well.

Martin KJELDSEN
Chief III

Hi guys,

Please find attached the l4r9-disco TouchGFX demo.

Hi @Martin KJELDSEN​ 

thanks a lot for providing the demo code =) , it will be very helpful for developing my application.

Best regards,

Christoph

Hi @Martin KJELDSEN​ ! Thanks a lot for procuring the source code for us! It'll be super helpful!