Skip to main content
Graduate
March 11, 2025
Question

Custom context in callback handlers

Hello,

I would like to request a feature to be added to the STM32 HAL.

Would it be possible to be able to add a custom user context when registering peripheral callbacks.

Example:

 

HAL_StatusTypeDef HAL_SPI_RegisterCallback(SPI_HandleTypeDef *hspi, HAL_SPI_CallbackIDTypeDef CallbackID, pSPI_CallbackTypeDef pCallback, void* UserContext);

 

And then as callback function:

 

typedef void (*pSPI_CallbackTypeDef)(SPI_HandleTypeDef *hspi, void* UserContext);

 

I really miss this feature and have had to code around it for god knows how many times.

I have added it myself to the SPI driver, but if I regenerate its all gone ofc.

So it would be real nice if this could be added to drivers.

 

Thx,

Alexander

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
March 11, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
March 12, 2025
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Pavel A.
March 11, 2025

> I have added it myself to the SPI driver, but if I regenerate its all gone 

To avoid losing your changes in the HAL libraries:

- When you use Cube to (re)generate code, select the option to create links to the libraries instead of copying all the files into your project. 

- Check your changes in the ST libraries into your version control (yes, make your private branch).

To minimize code differences, do not pass the UserContext as a new argument. Instead, add it to the SPI_HandleTypeDef struct. Then your callbacks will get this arg from the hspi pointer: hspi->UserContext.

 

 

Andrew Neil
Super User
March 11, 2025

@Pavel A. wrote:

To minimize code differences, do not pass the UserContext as a new argument. Instead, add it to the SPI_HandleTypeDef struct.


@Alexander4 there was some discussion of this in the 2021 thread:

https://community.st.com/t5/stm32-mcus-embedded-software/is-there-a-way-to-provide-context-pointer-to-hal-callback/m-p/182064

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
unsigned_char_array
Lead III
March 12, 2025

I agree it should have been added to the function argument or to the handler struct.

Alternatively you can create a mapping table.

Some pseudocode:

 

typedef void (*usercallback_t)(SPI_HandleTypeDef *hspi, void* usercontext);

typedef struct
{
 void *peripheral;
 void *usercontext;
 usercallback_t function;
} usercontext_mapping_t;

static usercontext_mapping_t mappingtable[N];

void callback(SPI_HandleTypeDef *hspi)
{
 if (hspi == NULL) return

 for(int i=0;i<N;++i)
 {
 if(mappingtable[i].peripheral == hspi->instance)
 {
 if (mappingtable[i].function != NULL)
 {
 mappingtable[i].function(hspi, mappingtable.usercontext);
 } 
 break;
 }
 }
}

 

 

Create a wrapper function around HAL_SPI_RegisterCallback that automatically registers the function and adds user context to the table. You can also wrap the deregister function.

I prefer creating wrapping functions over rewriting part of the functions. While it adds some overhead in terms of stack and CPU time that usually is not a problem. Once it becomes a problem I would switch from HAL to LL and write my own library.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."