cancel
Showing results for 
Search instead for 
Did you mean: 

[SOLVED] hal.initialize() causes hard fault. -- actually __libc_init_array() not called.

KShim.1738
Associate III

I'm porting toughgfx button example to rt-thread. I tested the environment with led blinking.

My environment is as below.

tool chains: scons + gas/gcc/g++

debugging : openocd + gdb

flash program : STM32CubeProgrammer with openjdk and openjfx

RTOS: rt-thread

Board: stm32f746g-disco

I merged the touchgfx button example into rt-thread. And then I began to experience a hard fault. It starts with touchgfx::touchgfx_init(). I checked that I have no problem with cpp codes, such as new operator and STL.

  at touchgfx-button/Middlewares/ST/TouchGFX/touchgfx/framework/include/common/TouchGFXInit.hpp:86

86     HAL& hal = getHAL<HALType>(dma, display, tc, width, height);

  at touchgfx-button/Middlewares/ST/TouchGFX/touchgfx/framework/include/common/TouchGFXInit.hpp:87

87     hal.initialize();

void OSWrappers::initialize()

0801c9a0 <_ZN8touchgfx3HAL10initializeEv>:

 801c9a0:    b510      push  {r4, lr}

 801c9a2:    4604      mov   r4, r0

 801c9a4:    f7f2 f986    bl   800ecb4 <_ZN8touchgfx10OSWrappers10initializeEv>

 801c9a8:    6860      ldr   r0, [r4, #4]

 801c9aa:    6803      ldr   r3, [r0, #0]

 801c9ac:    68db      ldr   r3, [r3, #12]

 801c9ae:    4798      blx   r3

After the call to OSWrappers::initialize(), r3 was 0x9db545a1.

 801c9ae:    4798      blx   0x9db545a1

For your information, my lds file is...

================= lds file =================

{

RAM (xrw)   : ORIGIN = 0x20000000, LENGTH = 320K

FLASH (rx)   : ORIGIN = 0x08000000, LENGTH = 1024K

QUADSPI (r)  : ORIGIN = 0x90000000, LENGTH = 16M

}

There should be no codes in QUADSPI area. But I don't know what that code is. Would you please advise me with my lds file?

I've enclosed the linker script file.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
LDoyl
Associate III

I had a hard fault error that came up when ever the external FLASH on a '469-Disco board was accessed. In the CubeIDE it looked like the data was in the FLASH -so what was the problem????

It turned out that STLINK could access the FLASH but the program couldn't. The clue to fixing this problem was the youtube https://www.youtube.com/watch?v=237lPdMsDZsL . I needed to copy files into the BSP folder for the touchscreen and QSPI FLASH which I copied from one of the demos. Also some of the parameters that CubeMX generated for the FLASH in the main.c appeared to be incorrect. These were replaced by the settings from the demo.

Hope this helps someone save some time.