2023-08-02 12:37 AM - edited 2023-08-02 12:59 AM
I store "FrontendHeap" to my external SDRAM and in the text appears question mark and when I want to change screen it crashes at specific screen.
I configured my SDRAM
void MX_FMC_Init(void)
{
/* USER CODE BEGIN FMC_Init 0 */
/* USER CODE END FMC_Init 0 */
FMC_SDRAM_TimingTypeDef SdramTiming = {0};
/* USER CODE BEGIN FMC_Init 1 */
/* USER CODE END FMC_Init 1 */
/** Perform the SDRAM1 memory initialization sequence
*/
hsdram1.Instance = FMC_SDRAM_DEVICE;
/* hsdram1.Init */
hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16;
hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2;
hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_2;
/* SdramTiming */
SdramTiming.LoadToActiveDelay = 2;
SdramTiming.ExitSelfRefreshDelay = 7;
SdramTiming.SelfRefreshTime = 5;
SdramTiming.RowCycleDelay = 7;
SdramTiming.WriteRecoveryTime = 3;
SdramTiming.RPDelay = 3;
SdramTiming.RCDDelay = 2;
if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
{
Error_Handler( );
}
/* USER CODE BEGIN FMC_Init 2 */
FMC_SDRAM_CommandTypeDef Command;
/* Step 1 and Step 2 already done in HAL_SDRAM_Init() */
/* Step 3: Configure a clock configuration enable command */
Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE; /* Set MODE bits to "001" */
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; /* configure the Target Bank bits */
Command.AutoRefreshNumber = 1;
Command.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
HAL_Delay(1); /* Step 4: Insert 100 us minimum delay - Min HAL Delay is 1ms */
/* Step 5: Configure a PALL (precharge all) command */
Command.CommandMode = FMC_SDRAM_CMD_PALL; /* Set MODE bits to "010" */
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
/* Step 6: Configure an Auto Refresh command */
Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE; /* Set MODE bits to "011" */
Command.AutoRefreshNumber = 2;
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
/* Step 7: Program the external memory mode register */
Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;/*set the MODE bits to "100" */
Command.ModeRegisterDefinition = (uint32_t)0 | 0<<3 | 2<<4 | 0<<7 | 1<<9;
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
/* Step 8: Set the refresh rate counter - refer to section SDRAM refresh timer register in RM0455 */
/* Set the device refresh rate
* COUNT = [(SDRAM self refresh time / number of row) x SDRAM CLK] – 20
= [(64ms/4096) * 100MHz] - 20 = 1562.5 - 20 ~ 1542 */
HAL_SDRAM_ProgramRefreshRate(&hsdram1, 1542);
/* USER CODE END FMC_Init 2 */
}
And MPU:
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_8MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0xC0300000;
MPU_InitStruct.Size = MPU_REGION_SIZE_2MB;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0xC0600000;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.BaseAddress = 0xC000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
MPU_InitStruct.AccessPermission = MPU_REGION_PRIV_RO;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
At 0xC0300000 and 0xC0600000 is framebuffers. at Cx0000000 is frontendheap. Maybe someone sees where problem is? When frontend heap is in the internal processor RAM it works fine
2023-08-02 1:19 AM
Hello
What if you set the heap area as non-cacheable in mmu config ?
Br J.T
2023-08-02 1:29 AM
Unfortunately, same..:sad_but_relieved_face:
2023-08-02 1:40 AM
Ok. Can you temporary disable the mmu to see its causing the problems ?
2023-08-02 2:15 AM
If I disable MPU it does not start at all.