2022-02-07 2:26 AM
2022-02-07 7:21 AM
Hi,
What version of TouchGFX are you using ? I guess you used a button with label ? Try to maybe delete the generated/ folder and regenerate code again.
/Romain
2022-02-07 8:26 AM
Hi Romain.
Yes, it is a button with label.
I already tried to do it, but in the new generated folder, there is still no files in the "generated\texts\include\texts" folder and there is no "generated\texts\src" folder at all.
2022-02-07 8:30 AM
BTW I use TouchGFX Designer 4.18.0
2022-12-23 1:16 AM
I have the same version fo the TouchGFX Designer and have had the same issue in the past. In some scenarios the designer fails to detect there is a change and does not regenerate the code correctly.
The trick to force a regeneration of the text is to make a small change to the container/screenthe T___SINGLEUSE is present.
For example if T___SINGLEUSE_73HN is used in a button change the text of the button, regenerate the text and set it back to the previous value. This will regenerate the texts.
It is clearly a bug from TouchgGFX