NUCLEO-F746ZG + 7" 800x480 SSD1963 16-bit FMC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 1:41 AM
I successfully implemented (via CubeMX) an application to manage the display.
So FMC initialization is correct, as are the prmitive to interact with the LCD
I would now like use TouchGFX.
I have read in the various posts that it can be done.
My problem is: where to start?
I have searched for a long time in the forum, but we are referring to older versions of the TouchGFX Designer.
The ideal would be an HowTo to create a Custom Application Template for a project generated with CubeMX and Atollic (or SW4STM32).
Solved! Go to Solution.
- Labels:
-
STM32F7 Series
-
TouchGFX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 6:02 AM
Okay, let me give you a super fast overview of what we need to do here without going into too many details:
- Configure RAM and flash memory - You've probably already done this.
- Configure the LTDC and Layer 1 (Maybe you've already done this)
- Configure TouchGFX with MCU specific (STM32F7) HAL, DMA, TouchController. Usually done in BoardConfiguration.cpp if you need inspiration from other applications. The TouchController is a hook in which you'll use your own drivers to sample touch over e.g. I2C.
- Create a gui task that runs the TouchGFX main event loop
- TouchGFX (and thus your application) will be driven by the VSYNC interrupt in STM32F7HAL.
Edit: Please have a look at https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-fmc
Let me know what you think and where you think we should start.
/Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 4:47 AM
Funny you should ask about this because i've just had a meeting with the product owner about writing an extensive article on porting TouchGFX to custom hardware platforms. We have articles but none that are very concise in a ST setup (CubeIDE, CubeMX, etc).
The "Creating a custom application template" is universal, though. It is not compiler specific: https://touchgfx.zendesk.com/hc/en-us/articles/115002741432-Create-custom-Application-Template.
CubeMX has its own issues but i'm headed somewhere next week to help fix some of the issues with integration.
I don't expect you can select TouchGFX for your Nucleo board? I'd write some pointers here, but i'm affraid it would get too complex too soon. I'd love to help, though. Let's start by figuring out what you can actually configure using CubeMX currently.
Let me know.
/Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 5:42 AM
Currently with the CubeMX I have configured FMC in 16-bit mode and related GPIOs for display control (reset, wait, interrupt).
The SSD1963 controller is correctly initialized and I can display graphics and text on the LCD.
I have already used TouchGFX on the STM32F746-DISCO and on the STM32F469I-DISCO (Atollic), but I need to go to a larger display (7 '' or 10.1 '').
I understand that it is currently possible only using boards that are already supported by TouchGFX Designer (such as EDT boards).
Another problem I have is that using internal controller of the micro (LTDC) many pins are used for LCD: the pins number usable for other devices goes down :crying_face:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 6:02 AM
Okay, let me give you a super fast overview of what we need to do here without going into too many details:
- Configure RAM and flash memory - You've probably already done this.
- Configure the LTDC and Layer 1 (Maybe you've already done this)
- Configure TouchGFX with MCU specific (STM32F7) HAL, DMA, TouchController. Usually done in BoardConfiguration.cpp if you need inspiration from other applications. The TouchController is a hook in which you'll use your own drivers to sample touch over e.g. I2C.
- Create a gui task that runs the TouchGFX main event loop
- TouchGFX (and thus your application) will be driven by the VSYNC interrupt in STM32F7HAL.
Edit: Please have a look at https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-fmc
Let me know what you think and where you think we should start.
/Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 7:18 AM
Sorry @Martin KJELDSEN​ ,
I did not understand point 2. : can I use LTDC in my scenario ? Or "LTDC and Layer 1" means "FMC"?
I would say starting from point 3.
For point 5 I was thinking (as read in other posts) of the TE pin (Tearing Effect Signale) of the SSD1963 controller.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-17 10:49 AM
How is your LCD connected? Being an STM32F7 i'd assume it has a TFT controller. Unrelated to FMC.
Okay, starting from point 3 i'll try to come up with a plan to follow. We'll have to take things step by step. Maybe the first thing to do is get a working project base - The things you have working now, are they in an Atollic project, and configured with CubeMX?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-18 12:04 AM
The LCD is connected as follow:
---- STM32 -------------------- SSD1963 ----------
PF0 FMC_A0 D/C - Data/Command Select
PD4 FMC_NOE RD# - 8080 Mode Read Strobe Signal
PD5 FMC_NWE WR# - 8080 Mode Write Strobe Signal
PD7 FMC_NE1 C/S - Chip Select
PD14 FMC_D0 DB0
PD15 FMC_D1 DB1
PD0 FMC_D2 DB2
PD1 FMC_D3 DB3
PE7 FMC_D4 DB4
PE8 FMC_D5 DB5
PE9 FMC_D6 DB6
PE10 FMC_D7 DB7
PE11 FMC_D8 DB8
PE12 FMC_D9 DB9
PE13 FMC_D10 DB10
PE14 FMC_D11 DB11
PE15 FMC_D12 DB12
PD8 FMC_D13 DB13
PD9 FMC_D14 DB14
PD10 FMC_D15 DB15
PC2 GPIO_OUT RESET - Master Syncronize Reset
PC0 GPIO_EXTI0 TE - Tearing Effect
PC3 GPIO_OUT BL - Backlight ON/OFF
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-04 3:11 AM
Hi Martin,
you have some news ?
In the meantime I bought the Waveshare Open746-I board, which have HW architecture very similar to ST32746-Discovey.
I hope you can give support on this.
P.S. I tried to contact EDT, but I didn't get a concrete answer!
Best Regards
Antonello
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-04 4:08 AM
Hi @Community member​,
What did you contact EDT about? Maybe i can help clarify with them. If you're using a configuration inspired by STM32F746-DISCO maybe you could start with an STM32F746-DISCO project (Start from the TGFX designer - V2.0.0 has an .ioc file for the board).
We should be able to start making necessary modifications from there on - Some settings and files used will be the same (e.g. STM32F7DMA- and -HAL.cpp)
How does that sound?
/Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-04 5:32 AM
I contacted EDT because they have cards with a 7 "and 10.1" display that support TouchGFX. that is similar to my HW scenario.
I would first start implementing my software before starting the HW design of my card.
I look forward to your extensive article on porting TouchGFX to custom hardware platforms :)
Thanks for the suggestions. As soon as the board arrives I will let you know.
Do you think the first step is to create an AT for the new/custom board ?
If I start with the tamplate for STM32F746-DISCO, how do I change LCD resolution (800x480)?
/Antonello