cancel
Showing results for 
Search instead for 
Did you mean: 

Many articles on touchGFX zendesk are unavailable since 3 weeks

LSant.1
Associate II

There where so many touchgfx help articles at https://touchgfx.zendesk.com/ .

e.g. memory requirements for touchgfx

Where are these articles?

If i use the bookmarks from my browser i only get:

0690X00000BwES4QAN.png

For this url for example: https://touchgfx.zendesk.com/hc/en-us/articles/205362991-TouchGFX-memory-requirements

Is their a way to find these old articles? I found them very helful and i set many bookmarks in my browser to these pages. And when i search from google they are stil referenced.

Would be great to get them back.

1 ACCEPTED SOLUTION

Accepted Solutions
Martin KJELDSEN
Chief III

Some have been taken down since they're either inaccurate given the current state of integration with CubeMX or confusing or simply not good enough. If you have any specific requirements, i'll share the articles with you - Voila!

As @HP​ says, we're writing new documentation for a different platform (to get rid of zendesk). 90% of the office is involved in this effort.

View solution in original post

7 REPLIES 7
HP
Senior III

As far as I've heard TouchGFX is transitioning from ZenDesk to another system. that could explain why the articles have gone missing.

As for finding them one option could be to use archive.org. Maybe not optimal but my bet is that the new documentation is going through some substantial changes and it will be worth waiting for. I think the whole TouchGFX team is running flat out (and have been for quite some time) so the best is to wait a little and see what happens 🙂

Martin KJELDSEN
Chief III

Some have been taken down since they're either inaccurate given the current state of integration with CubeMX or confusing or simply not good enough. If you have any specific requirements, i'll share the articles with you - Voila!

As @HP​ says, we're writing new documentation for a different platform (to get rid of zendesk). 90% of the office is involved in this effort.

LSant.1
Associate II

@Martin KJELDSEN​ thanks a lot for that.

Their are some other documents i would like to have

-Setting up CubeMX für STM32F429 Disco

https://touchgfx.zendesk.com/hc/en-us/articles/360021620431-Configuring-STM32F429I-DISCO

-using touchgfx without rtos

https://touchgfx.zendesk.com/hc/en-us/articles/204887741-Running-TouchGFX-without-an-operating-system

-integrating cubeMX and TouchGFX

https://touchgfx.zendesk.com/hc/en-us/articles/360006678572-Integrating-CubeMX-and-TouchGFX

Its good to know that the documentation is renewed

Kind Regards

Martin KJELDSEN
Chief III

Yes, we're spending a ton of effort on this it feels. Previously, we'd do "budding" articles which clouded the overall overview of touchgfx. Now that we're in CubeMX, etc, we felt it was time to have another iteration on a different platform.

Martin KJELDSEN
Chief III
 
Martin KJELDSEN
Chief III
 
Martin KJELDSEN
Chief III

This is for CubeMX 5.4, though, hence why it was taken down. TouchGFX Generator (CubeMX 5.5) does things in a different way. Maybe you can get some inspiration, though.