2022-05-11 12:37 AM
When I set up contrast to value less than 5 I get stuck on HAL_LCD_Init() on wait for booster, and initialization fails:
/*!< Wait Until the LCD Booster is ready */
while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_RDY) == RESET)
{
if((HAL_GetTick() - tickstart ) > LCD_TIMEOUT_VALUE)
{
hlcd->ErrorCode = HAL_LCD_ERROR_RDY;
return HAL_TIMEOUT;
}
}
Do I have to initilize something else to get other values of contrast?
hlcd.Instance = LCD;
hlcd.Init.Prescaler = LCD_PRESCALER_1;
hlcd.Init.Divider = LCD_DIVIDER_31;
hlcd.Init.Duty = LCD_DUTY_1_4;
hlcd.Init.Bias = LCD_BIAS_1_3;
hlcd.Init.VoltageSource = LCD_VOLTAGESOURCE_INTERNAL;
hlcd.Init.Contrast = LCD_CONTRASTLEVEL_5;
hlcd.Init.DeadTime = LCD_DEADTIME_0;
hlcd.Init.PulseOnDuration = LCD_PULSEONDURATION_4;
hlcd.Init.HighDrive = LCD_HIGHDRIVE_0;
hlcd.Init.BlinkMode = LCD_BLINKMODE_OFF;
hlcd.Init.BlinkFrequency = LCD_BLINKFREQUENCY_DIV8;
hlcd.Init.MuxSegment = LCD_MUXSEGMENT_DISABLE;
2024-03-20 6:05 AM
I al facing similar to above issue. I could not able to configure the internal voltage source. The while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_RDY) == RESET) never sets if the internal voltage source is selected. My configurations are listed below,
hlcd.Instance = LCD;
hlcd.Init.Prescaler = LCD_PRESCALER_1;
hlcd.Init.Divider = LCD_DIVIDER_31;
hlcd.Init.Duty = LCD_DUTY_1_4;
hlcd.Init.Bias = LCD_BIAS_1_3;
hlcd.Init.VoltageSource = LCD_VOLTAGESOURCE_INTERNAL;
hlcd.Init.Contrast = LCD_CONTRASTLEVEL_6;
hlcd.Init.DeadTime = LCD_DEADTIME_0;
hlcd.Init.PulseOnDuration = LCD_PULSEONDURATION_4;
hlcd.Init.HighDrive = LCD_HIGHDRIVE_0;
hlcd.Init.MuxSegment = LCD_MUXSEGMENT_DISABLE;
hlcd.Init.BlinkMode = LCD_BLINKMODE_OFF;
hlcd.Init.BlinkFrequency = LCD_BLINKFREQUENCY_DIV8;
Anybody faced similar issue. Anyone can support for solution