cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L073 about LCD Set-up Convertor when setting LCD_VOLTAGESORCE_INTERNAL. The set voltage and measured voltage are different.

R.K
Associate II

Hello Developper Teams.

I use STM32L073.

About LCD Setting, The set voltage and measured voltage are different.

​For example,  hlcd.Init.Contrast = LCD_CONTRASTLEVEL_0(2.6V) --> Measured voltage = 3.7V

Is there another place to set it?

​Setting HD=1 dropped it down to 3V, but I can't understand it out.

Is it compatible with LCD specifications?

Best regard.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Is it possible that you have this problem using the NUCLEO-L073RZ?

In this case, you should definitely take a look at the schematics, because there you can see that VLCD (pin 1) is connected to VDD via SB45. Please don't get confused there, because since the underlying board MB1136 is also used for other STM32s, pin 1 has the designation VBAT/VLCD, whereas VBAT is not relevant for the STM32L073.

After desoldering SB45, everything should work as desired.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.