2020-06-26 10:50 PM
Hello,
I am new to Touch GFX. I have build a GUI in touch Gfx and then generated the code.
But when I tried to compile the generated code in Keil IDE , It shows the following errors
Build started: Project: STM32F769I_DISCO
*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'STM32F769I_DISCO'
Clean started - Project: 'STM32F769I_DISCO'
deleting intermediate output files for target 'STM32F769I_DISCO'
assembling startup_stm32f769xx.s...
compiling CortexMMCUInstrumentation.cpp...
../TouchGFX/target/CortexMMCUInstrumentation.hpp(4): error: #5: cannot open source input file "platform/core/MCUInstrumentation.hpp": No such file or directory
#include <platform/core/MCUInstrumentation.hpp>
../TouchGFX/target/CortexMMCUInstrumentation.cpp: 0 warnings, 1 error
compiling Buttons.cpp...
../TouchGFX/target/Buttons.cpp(39): error: #5: cannot open source input file "touchgfx/hal/Buttons.hpp": No such file or directory
#include <touchgfx/hal/Buttons.hpp>
../TouchGFX/target/Buttons.cpp: 0 warnings, 1 error
compiling KeySampler.cpp...
../TouchGFX/target/KeySampler.hpp(42): error: #5: cannot open source input file "platform/driver/button/ButtonController.hpp": No such file or directory
#include <platform/driver/button/ButtonController.hpp>
../TouchGFX/target/KeySampler.cpp: 0 warnings, 1 error
compiling TouchGFXHAL.cpp...
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp(20): error: #5: cannot open source input file "touchgfx/hal/HAL.hpp": No such file or directory
#include <touchgfx/hal/HAL.hpp>
../TouchGFX/target/TouchGFXHAL.cpp: 0 warnings, 1 error
compiling STM32TouchController.cpp...
../TouchGFX/target/STM32TouchController.hpp(23): error: #5: cannot open source input file "platform/driver/touch/TouchController.hpp": No such file or directory
#include <platform/driver/touch/TouchController.hpp>
../TouchGFX/target/STM32TouchController.cpp: 0 warnings, 1 error
compiling TouchGFXGPIO.cpp...
../TouchGFX/target/TouchGFXGPIO.cpp(18): error: #5: cannot open source input file "touchgfx/hal/GPIO.hpp": No such file or directory
#include <touchgfx/hal/GPIO.hpp>
../TouchGFX/target/TouchGFXGPIO.cpp: 0 warnings, 1 error
compiling TouchGFXConfiguration.cpp...
../TouchGFX/target/generated/TouchGFXConfiguration.cpp(17): error: #5: cannot open source input file "texts/TypedTextDatabase.hpp": No such file or directory
#include <texts/TypedTextDatabase.hpp>
../TouchGFX/target/generated/TouchGFXConfiguration.cpp: 0 warnings, 1 error
compiling TouchGFXGeneratedHAL.cpp...
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp(20): error: #5: cannot open source input file "touchgfx/hal/HAL.hpp": No such file or directory
#include <touchgfx/hal/HAL.hpp>
../TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp: 0 warnings, 1 error
compiling STM32DMA.cpp...
../TouchGFX/target/generated/STM32DMA.cpp(20): error: #5: cannot open source input file "touchgfx/hal/OSWrappers.hpp": No such file or directory
#include <touchgfx/hal/OSWrappers.hpp>
../TouchGFX/target/generated/STM32DMA.cpp: 0 warnings, 1 error
compiling OSWrappers.cpp...
../TouchGFX/target/generated/OSWrappers.cpp(17): error: #5: cannot open source input file "touchgfx/hal/OSWrappers.hpp": No such file or directory
I don't understand whats the issue with the generated code. I have not change any line of code just build it as it was generated.
Please help
Regards
Manvendra
#include <touchgfx/hal/OSWrappers.hpp>
../TouchGFX/target/generated/OSWrappers.cpp: 0 warnings, 1 error
Solved! Go to Solution.
2020-07-11 7:29 AM
Hello,
When you create a project the IDE by default is CubeIDE.
In order to make Keil compile, you need to specify in CubeMX (opening the .ioc file) the right IDE.
For that:
/Alexandre
2020-07-11 12:46 AM
Hello,
It seems that the TouchGFX framework is not correctly installed.
Can you enumerate the steps you did to arrive to this ?
/Alexandre
2020-07-11 5:42 AM
Hello Alexandre RENOUX ,
Thanks for your response.
Here are the steps which I am following
Regards,
Manvendra
2020-07-11 7:29 AM
Hello,
When you create a project the IDE by default is CubeIDE.
In order to make Keil compile, you need to specify in CubeMX (opening the .ioc file) the right IDE.
For that:
/Alexandre
2020-07-12 10:56 PM
Hello,
Thanks for your response.
I followed your points. And now it is giving another error, It seems the installed compiler doesn't support C++.
Build started: Project: STM32F769I_DISCO
*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
*** Warning: You are compiling one or more files of source type C++ and have selected 'use MicroLIB'. MicroLIB does not support C++!
Build target 'STM32F769I_DISCO'
assembling startup_stm32f769xx.s...
compiling TouchGFXHAL.cpp...
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp(20): error: #5: cannot open source input file "touchgfx/hal/HAL.hpp": No such file or directory
#include <touchgfx/hal/HAL.hpp>
../TouchGFX/target/TouchGFXHAL.cpp: 0 warnings, 1 error
compiling STM32TouchController.cpp...
../TouchGFX/target/STM32TouchController.hpp(23): error: #5: cannot open source input file "platform/driver/touch/TouchController.hpp": No such file or directory
#include <platform/driver/touch/TouchController.hpp>
../TouchGFX/target/STM32TouchController.cpp: 0 warnings, 1 error
compiling TouchGFXGPIO.cpp...
../TouchGFX/target/TouchGFXGPIO.cpp(18): error: #5: cannot open source input file "touchgfx/hal/GPIO.hpp": No such file or directory
#include <touchgfx/hal/GPIO.hpp>
../TouchGFX/target/TouchGFXGPIO.cpp: 0 warnings, 1 error
compiling CortexMMCUInstrumentation.cpp...
../TouchGFX/target/CortexMMCUInstrumentation.hpp(4): error: #5: cannot open source input file "platform/core/MCUInstrumentation.hpp": No such file or directory
#include <platform/core/MCUInstrumentation.hpp>
../TouchGFX/target/CortexMMCUInstrumentation.cpp: 0 warnings, 1 error
compiling Buttons.cpp...
../TouchGFX/target/Buttons.cpp(39): error: #5: cannot open source input file "touchgfx/hal/Buttons.hpp": No such file or directory
#include <touchgfx/hal/Buttons.hpp>
../TouchGFX/target/Buttons.cpp: 0 warnings, 1 error
compiling TouchGFXConfiguration.cpp...
../TouchGFX/target/generated/TouchGFXConfiguration.cpp(17): error: #5: cannot open source input file "texts/TypedTextDatabase.hpp": No such file or directory
#include <texts/TypedTextDatabase.hpp>
../TouchGFX/target/generated/TouchGFXConfiguration.cpp: 0 warnings, 1 error
compiling KeySampler.cpp...
../TouchGFX/target/KeySampler.hpp(42): error: #5: cannot open source input file "platform/driver/button/ButtonController.hpp": No such file or directory
#include <platform/driver/button/ButtonController.hpp>
../TouchGFX/target/KeySampler.cpp: 0 warnings, 1 error
compiling TouchGFXGeneratedHAL.cpp...
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp(20): error: #5: cannot open source input file "touchgfx/hal/HAL.hpp": No such file or directory
#include <touchgfx/hal/HAL.hpp>
../TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp: 0 warnings, 1 error
compiling OSWrappers.cpp...
../TouchGFX/target/generated/OSWrappers.cpp(17): error: #5: cannot open source input file "touchgfx/hal/OSWrappers.hpp": No such file or directory
#include <touchgfx/hal/OSWrappers.hpp>
../TouchGFX/target/generated/OSWrappers.cpp: 0 warnings, 1 error
compiling STM32DMA.cpp...
../TouchGFX/target/generated/STM32DMA.cpp(20): error: #5: cannot open source input file "touchgfx/hal/OSWrappers.hpp": No such file or directory
#include <touchgfx/hal/OSWrappers.hpp>
../TouchGFX/target/generated/STM32DMA.cpp: 0 warnings, 1 error
compiling main.c...
compiling freertos.c...
compiling stm32f7xx_it.c...
compiling stm32f7xx_hal_timebase_tim.c...
compiling stm32f7xx_hal_msp.c...
compiling stm32f7xx_hal_cortex.c...
compiling stm32f7xx_hal_crc_ex.c...
compiling stm32f7xx_hal_crc.c...
compiling stm32f7xx_hal_rcc.c...
compiling stm32f7xx_hal_flash.c...
compiling stm32f7xx_hal_rcc_ex.c...
compiling stm32f7xx_hal_flash_ex.c...
compiling stm32f7xx_hal_gpio.c...
compiling stm32f7xx_hal_dma_ex.c...
compiling stm32f7xx_hal_dma.c...
compiling stm32f7xx_hal_pwr_ex.c...
compiling stm32f7xx_hal_pwr.c...
compiling stm32f7xx_hal.c...
compiling stm32f7xx_hal_i2c_ex.c...
compiling stm32f7xx_hal_exti.c...
compiling stm32f7xx_hal_dma2d.c...
compiling stm32f7xx_hal_i2c.c...
compiling stm32f7xx_hal_dsi.c...
compiling stm32f7xx_hal_sdram.c...
compiling stm32f7xx_ll_fmc.c...
compiling stm32f7xx_hal_ltdc_ex.c...
compiling stm32f7xx_hal_ltdc.c...
compiling stm32f7xx_hal_qspi.c...
compiling system_stm32f7xx.c...
compiling stm32f7xx_hal_tim_ex.c...
compiling croutine.c...
compiling event_groups.c...
compiling list.c...
compiling stm32f7xx_hal_tim.c...
compiling queue.c...
compiling stream_buffer.c...
compiling tasks.c...
compiling timers.c...
compiling heap_4.c...
compiling port.c...
compiling cmsis_os2.c...
"STM32F769I_DISCO\STM32F769I_DISCO.axf" - 10 Error(s), 0 Warning(s).
Target not created.
Build Time Elapsed: 00:00:06
Regards
Manvendra
2020-07-13 1:18 AM
Hello,
The warning saying "MicroLIB does not support C++" is not important. This should not create the generated errors.
I have the impression that the include paths are not correctly defined in your project.
Are you sure you generated code with TouchGFX Designer before compiling in Keil ?
Can you check your include paths in your project ?
/Alexandre