‎2019-09-27 10:11 AM
Hello,
I ported the first example in the article "Interfacing with hardware in TouchGFX Applications" to TouchGFX Designer V4.10 and then ported it to STM32CubeIDE V1.0.2.
Please find it in attachment. I hope you find it helpful.
I didn't use the ioc and I am not sure its gonna work.
Board: STM32F746G-DISCO
Tools:
IAR EWARM V8.40.1
STM32CubeIDE V1.0.2
STM32CubeProgrammer V2.1.0
Note: STM32CubeIDE doesn't load the assets to the external memory. You need STM32CubeProgrammer having the external loader "N25Q128A_STM32F746G-DISCO" selected to load the assets.
With regards,
Badreddine
‎2019-09-30 1:19 AM
Hi @AME MCU Support Center BB​,
Thanks for the contribution!
/Martin
‎2019-09-30 4:48 PM
‎2019-10-01 12:25 AM
Thanks! =) I've talk to Soren about gathering all these contributions somewhere central so it's easy for people to get an overview.
/Martin