cancel
Showing results for 
Search instead for 
Did you mean: 

I want to debug STM32F769I-DISCO

Ebun.1
Senior

Hello.

environment

STM32CubeIDE Ver1.3.0

STM32CubeMX Ver5.5.0

TouchGFX Ver4.13.0

Double-click the following .project created by TouchGFX to start the IDE.

Build is OK.

After that, when Run-Debug, the following error message appears and it does not work.

What should I do?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

I have also seen this error if the external loader is not functioning correctly. I have also seen it when the linker definition file is not correct. there are a number of possibilities.

View solution in original post

5 REPLIES 5
Martin KJELDSEN
Chief III

You need to add an external flashloader to your project. You can do that from the project settings.

/Martin

Dear Martin

Thank you for helping.

Configured as attached in Debug Configurations.

The result is the same.

What to check next?

Thank you.

I have also seen this error if the external loader is not functioning correctly. I have also seen it when the linker definition file is not correct. there are a number of possibilities.

Ebun.1
Senior

Dear ScottSD

Editing the linker script solved

Thank you very much.

Awesome!

Glad I could help.