2021-05-27 6:56 PM
Question:
When touchgfx designer selects extflash, the screen is black, and it is normal to switch to intflash。。。。
I feel incredible,can't find out the cause of the problem:tired_face:
Do I need to modify any files of touchgfx?
***.sct:
LR_IROM1 0x08000000 0x00200000 { ; load region size_region
ER_IROM1 0x08000000 0x00200000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x20000000 0x00040000 { ; RW data
.ANY (+RW +ZI)
}
RW_FRAMEBUFFER 0x20040000 UNINIT 0x00060000 { ; RW data framebuffer
; Allocating region to framebuffer
}
}
LR_EROM1 0x90000000 0x4000000 { ; load region size_region
ER_EROM1 0x90000000 0x4000000 { ; load address = execution address
*.o (ExtFlashSection)
*.o (TextFlashSection)
*.o (FontFlashSection)
}
}