TOUCHGFX4.16.1 run target failed
... Compile
make -f ../gcc/Makefile -j8
Reading TouchGFX/application.config
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
Done
Flash
make -f ../gcc/Makefile flash -j8
Reading TouchGFX/application.config
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
d:/touchgfx_test/MyApplication_13/gcc/include/flash_sections_int_ext.mk:2: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 5
make: *** [flash] Error 2
../gcc/Makefile:52: recipe for target 'flash' failed
Failed
Failed
ps:
STM32F746G_ DISCO board.
touchgfx set up at D:\TouchGFX\4.16.1.
stm32cubeprogrammer set up at D:\Program .Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer (the latest 2.7.0 version)
The firmware version of ST- LINK is v2J37M27.
D:\touchgfx_test\MyApplication_13\gcc\include\cube_programmer.mk line 7&8
program_files_win32 = /c/Program Files (x86) --> program_files_win32 = /d/Program Files (x86)
program_files_win64 = /c/Program Files --> program_files_win64 = /d/Program Files
Using the stm32cubeprogrammer sofeware, open D:\touchgfx_test\MyApplication_13\TouchGFX\build\bin\target.hex, download, It is ok.