2024-02-07 11:16 PM - last edited on 2024-02-09 2:02 AM by LouisB
Hello everyone, I hope you are all having a great day. I would like to know how to work with the labels for the dynamic graph widget :
I want to know how to make the X axis labels display a real time value instead of numbers and I want it to be accurate to the real time, for example : Instead of 10,20 etc I want it to show 01:10 AM, 01:20 AM. etc. can someone help me with this please? Thank You Best Regards.
Solved! Go to Solution.
2024-02-08 9:44 AM - edited 2024-02-09 8:44 AM
Hi
I think you cannot get time to the X labels directly from TGFX Designer:slightly_frowning_face:
You need to litte bit manipulate the GraphLabels.cpp (and maybe be GraphLabels.hpp, depends on what you want).
Browse first to \Middlewares\ST\touchgfx\framework\source\touchgfx\widgets\graph\ folder and copy GraphLabels.cpp to your project \TouchGFX\gui\src\common\ folder for example.Edit that copy in \common\ folder.
Here is simple example which prints hh:mm AM/PM format time when number of decimals is set to value 4 in TGFX designer for X Labels.
GraphLabels.cpp:
void GraphLabelsBase::formatLabel(Unicode::UnicodeChar* buffer, int16_t bufferSize, int label, int decimals, Unicode::UnicodeChar decimalPoint, int scale) const
{
int length = 0;
int scaledLabel;
if (label < 0 && length < bufferSize - 1)
{
buffer[length++] = '-';
label = -label;
}
if (decimals == 0)
{
scaledLabel=(label + scale / 2) / scale;
Unicode::snprintf(buffer + length, bufferSize - length, "%d", (label + scale / 2) / scale);
}
/* HERE Simply Extension to print X label time */
else if (decimals == 4) // custom print time hh:mm AM when set 4 decimal in the TGFX designer
{
scaledLabel=label;
// cut down the overflow (24 hours * 60 minutes)
scaledLabel%=(24*60);
if(scaledLabel<(12*60))
Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d AM", scaledLabel/60,scaledLabel%60);
else
Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d PM", scaledLabel/60,scaledLabel%60);
}
else if (decimals > 0)
{
Unicode::snprintf(buffer + length, bufferSize - length, "%d", label / scale);
length = Unicode::strlen(buffer);
if (length < bufferSize - 1)
{
buffer[length++] = decimalPoint;
int remainder = label % scale;
for (int i = 0; i < decimals && length < bufferSize - 1; i++)
{
remainder *= 10;
if (i == decimals - 1 || length == bufferSize - 1)
{
remainder += scale / 2; // Rounding on the last (visible) digit
}
const int digit = (remainder / scale);
buffer[length++] = (Unicode::UnicodeChar)('0' + digit);
remainder %= scale;
}
buffer[length] = (Unicode::UnicodeChar)0;
}
}
}
Note that if you do like this, one point must represent value of one minute in your data to get time domain correct !
Then, your data will naturally start from time 00:00
Which is not allways the case. One way might be to add offset for starting time. So browse to \Middlewares\ST\touchgfx\framework\include\touchgfx\widgets\graph\- folder and open GraphLabels.hpp.
Add variable labelOffset and funtion 'setXStartOffset' to the X labels class.
GraphLabels.hpp:
class GraphLabelsX : public GraphLabelsBase
{
public:
/** EXTENSION:
* Variable for X -label offset , when using extended time- type X labels
*
*/
int labelOffset=0;
/** EXTENSION:
* Function for set X -label offset
*
* offset The X label offset of first the label value
*/
virtual void setXStartOffset(int offset)
{
labelOffset=offset;
}
virtual void invalidateGraphPointAt(int16_t index);
Then open GraphLabels.cpp and locate GraphLabelsX::drawString- funtion. Add summing of labelOffset to the call of formatLabel. (Note that same format routine is called for X and Y labels, so this offset must be take into account here in the call).
GraphLabels.cpp:
void GraphLabelsX::drawString(const Rect& invalidatedArea, const Font* fontToDraw, const AbstractDataGraph* graph, const int valueScaled, const int labelScaled, const uint8_t a) const
{
const int16_t labelX = valueToScreenXQ5(graph, valueScaled).round() - graph->getGraphAreaPaddingLeft();
if (labelX < 0 || labelX >= graph->getGraphAreaWidth())
{
return;
}
Unicode::UnicodeChar wildcard[20];
/*** Extension HERE - labelOffset summed with label- value: */
formatLabel(wildcard, 20, labelOffset+getIndexToXAxis(graph, valueScaled, labelScaled), labelDecimals, labelDecimalPoint, graph->getScaleX());
// Adjust to make label centered
int16_t labelWidth;
const Unicode::UnicodeChar* text = labelTypedText.getText();
Then you can set in your view.cpp something like
dynamicGraph1MajorXAxisLabel.setXStartOffset((11*60)+45); //11:45 AM
And then time starts from 11:45 AM
Here are the most important settings of graph in this example:
Number of decimals is set to 4 to activate extended time formatting for X labels. Since the Y label uses the same formatLabel function, there is must something that activates Time format for x labels but not for y (in most cases not needed to have time also in Y label).
This is just simple example how to extend DynamicGraph.
Hope this helps somebody.
Br JTP
2024-02-08 9:44 AM - edited 2024-02-09 8:44 AM
Hi
I think you cannot get time to the X labels directly from TGFX Designer:slightly_frowning_face:
You need to litte bit manipulate the GraphLabels.cpp (and maybe be GraphLabels.hpp, depends on what you want).
Browse first to \Middlewares\ST\touchgfx\framework\source\touchgfx\widgets\graph\ folder and copy GraphLabels.cpp to your project \TouchGFX\gui\src\common\ folder for example.Edit that copy in \common\ folder.
Here is simple example which prints hh:mm AM/PM format time when number of decimals is set to value 4 in TGFX designer for X Labels.
GraphLabels.cpp:
void GraphLabelsBase::formatLabel(Unicode::UnicodeChar* buffer, int16_t bufferSize, int label, int decimals, Unicode::UnicodeChar decimalPoint, int scale) const
{
int length = 0;
int scaledLabel;
if (label < 0 && length < bufferSize - 1)
{
buffer[length++] = '-';
label = -label;
}
if (decimals == 0)
{
scaledLabel=(label + scale / 2) / scale;
Unicode::snprintf(buffer + length, bufferSize - length, "%d", (label + scale / 2) / scale);
}
/* HERE Simply Extension to print X label time */
else if (decimals == 4) // custom print time hh:mm AM when set 4 decimal in the TGFX designer
{
scaledLabel=label;
// cut down the overflow (24 hours * 60 minutes)
scaledLabel%=(24*60);
if(scaledLabel<(12*60))
Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d AM", scaledLabel/60,scaledLabel%60);
else
Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d PM", scaledLabel/60,scaledLabel%60);
}
else if (decimals > 0)
{
Unicode::snprintf(buffer + length, bufferSize - length, "%d", label / scale);
length = Unicode::strlen(buffer);
if (length < bufferSize - 1)
{
buffer[length++] = decimalPoint;
int remainder = label % scale;
for (int i = 0; i < decimals && length < bufferSize - 1; i++)
{
remainder *= 10;
if (i == decimals - 1 || length == bufferSize - 1)
{
remainder += scale / 2; // Rounding on the last (visible) digit
}
const int digit = (remainder / scale);
buffer[length++] = (Unicode::UnicodeChar)('0' + digit);
remainder %= scale;
}
buffer[length] = (Unicode::UnicodeChar)0;
}
}
}
Note that if you do like this, one point must represent value of one minute in your data to get time domain correct !
Then, your data will naturally start from time 00:00
Which is not allways the case. One way might be to add offset for starting time. So browse to \Middlewares\ST\touchgfx\framework\include\touchgfx\widgets\graph\- folder and open GraphLabels.hpp.
Add variable labelOffset and funtion 'setXStartOffset' to the X labels class.
GraphLabels.hpp:
class GraphLabelsX : public GraphLabelsBase
{
public:
/** EXTENSION:
* Variable for X -label offset , when using extended time- type X labels
*
*/
int labelOffset=0;
/** EXTENSION:
* Function for set X -label offset
*
* offset The X label offset of first the label value
*/
virtual void setXStartOffset(int offset)
{
labelOffset=offset;
}
virtual void invalidateGraphPointAt(int16_t index);
Then open GraphLabels.cpp and locate GraphLabelsX::drawString- funtion. Add summing of labelOffset to the call of formatLabel. (Note that same format routine is called for X and Y labels, so this offset must be take into account here in the call).
GraphLabels.cpp:
void GraphLabelsX::drawString(const Rect& invalidatedArea, const Font* fontToDraw, const AbstractDataGraph* graph, const int valueScaled, const int labelScaled, const uint8_t a) const
{
const int16_t labelX = valueToScreenXQ5(graph, valueScaled).round() - graph->getGraphAreaPaddingLeft();
if (labelX < 0 || labelX >= graph->getGraphAreaWidth())
{
return;
}
Unicode::UnicodeChar wildcard[20];
/*** Extension HERE - labelOffset summed with label- value: */
formatLabel(wildcard, 20, labelOffset+getIndexToXAxis(graph, valueScaled, labelScaled), labelDecimals, labelDecimalPoint, graph->getScaleX());
// Adjust to make label centered
int16_t labelWidth;
const Unicode::UnicodeChar* text = labelTypedText.getText();
Then you can set in your view.cpp something like
dynamicGraph1MajorXAxisLabel.setXStartOffset((11*60)+45); //11:45 AM
And then time starts from 11:45 AM
Here are the most important settings of graph in this example:
Number of decimals is set to 4 to activate extended time formatting for X labels. Since the Y label uses the same formatLabel function, there is must something that activates Time format for x labels but not for y (in most cases not needed to have time also in Y label).
This is just simple example how to extend DynamicGraph.
Hope this helps somebody.
Br JTP
2024-02-28 11:27 PM
Hello all,
Just don't forget to add wildcard characters to your topography with JTP1's solution :
Regards,