cancel
Showing results for 
Search instead for 
Did you mean: 

How to create a Touchgfx project for the ST Boards which are not listed on the Board selector of TouchDesigner

KGupt.1
Associate III

I want to create a custom Touchghx project for the STM32F746MCU it has an LCD TFT screen based on the MIPI-DSI interface.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

TouchGFXDesigner isnt application to generate projects. Here you can generate only examples.

Normal way is generate project in MX or MX IDE and manage it in designer.