2022-03-03 7:05 AM
I know that the touch screen is reversed in one direction from the Disc to the Disc1. Are there any other differences? I want to use a couple of I/O pins for a project and need to know which ones are available.
2022-03-03 9:18 AM
Welcome, @SGill.3 to the community!
the STM32F429I-DISC1 is almost identical to the STM32F429I-DISCO, except:
From TouchGFX's point of view, both boards are otherwise identical.
Does it answer your question?
Regards
/Peter
2022-03-03 9:31 AM
@Peter BENSCH ,
> From TouchGFX's point of view, both boards are otherwise identical.
No, they are not - as @SGill.3 said, the touchscreen is mirrored in the longer axis.
If you have both versions at hand, you can try the simple "doodle" program I gave link to in that thread; and also the test program generated by TouchGFX, posted by Raymond in the parallel thread https://www.eevblog.com/forum/microcontrollers/need-hex-file-to-test-touch-screen-on-stm32f429-discovery-board/ (where dmendesf confirmed the flip).
JW
2022-03-03 10:00 AM
The information about the pins is what I was looking for.
I have asked before if there was someway to flip the touch screen in the software, but did not get a good answer.
SG
2022-03-06 11:29 PM
@Community member
Thanks for the information. Unfortunately, I don't have the new version at hand, so I can't check or confirm this directly. As soon as I have one, I'll be happy to do so.
Regards
/Peter
2022-03-08 1:08 AM
Hi Peter,
Apparently, TouchGFX crew have the new version and build for that, so you should see the "mirroring" effect on the old version - just for the fun of it, you can try one of the firmwares posted by Raymond on eevblog.
Jan
#TouchGFX