cancel
Showing results for 
Search instead for 
Did you mean: 

How to change TouchGFX Windows simulation icons?

VSimu.1
Associate III

How do we change the TouchGFX Windows simulation icon?

See "how" image. I want to change the icon that appears in the top-left corner of the window, as well as the icon that appears in the windows task bar.

I can see that the icon used for these is located at

C:\TouchGFX\4.13.0\designer\Skins\Dark\Logo\touchgfx_logo.png

C:\TouchGFX\4.13.0\designer\Skins\Blue\Logo\touchgfx_logo.png

But if I manually change these and run the TouchGFX Simulator, the icon does not change. Where is this hard-coded then, so that we can change this?

I also see that the "touchgfx_logo.png" file is referenced in these files

C:\TouchGFX\4.13.0\designer\Skins\Dark\skin.json

C:\TouchGFX\4.13.0\designer\Skins\Blue\skin.json

in the line:  "Image": "Logo/touchgfx_logo.png", in lines 1512 and 1513 respectfully.

We have also found this file, but this icon is completely different than these:

C:\TouchGFX\4.13.0\designer\Files\touchgfx.ico

We are using TouchGFX version 4.13.0 if this was not clear from the folder paths.

Can we change this or is this impossible to change? :artist_palette:

3 REPLIES 3
Martin KJELDSEN
Chief III

The icon used by the simulator is taken from, e.g..

C:\TouchGFX\4.13.0\designer\Files

And once the application is created it is located in the following folder of your app:

TouchGFX\simulator

/Martin

VSimu.1
Associate III

Thank you very for your reply. I was able to change how the icon appears in windows explorer.

Could you please take a look at the 2 orange circles? I am also trying to change those 2 icons. The icon of the top-left corner of the window, and the icon that appears on the windows task bar.

Could you please tell me how to change those as well?

See attached "how3"

Hello, any follow up information to the post below? Any info is appreciated.