cancel
Showing results for 
Search instead for 
Did you mean: 

STemWin5.44 lib missing GUI_SPLINE functions

APort
Associate III

Hello,

Latest version of STemWin as included in STM32Cube_FW_L4_V1.14.0 apparently missing GUI_SPLINE_* functions in the provided *.a libs but they are listed in header file (GUI.h) - which causes linking error.

We are working with STemWin_CM4_wc32_ot_ARGB.a in particular but others are missing it as well.

This is very important feature for us.

Is there newer version, or version with this feature working?

Thanks in advance

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
CSage
Associate

Hej,

Could you solve this issue?

I´m using STM32Cube_FW_F4_V1.24.2. This results into the same issue. I´m also using the same lib STemWIN_CM4_OS_wc32_ot_ARGB.a.