2021-04-16 1:31 PM
Hello,
I have made a custom board based around the STM32F746IGT6 MCU to run a 800x480 display 7in (4DLCD-70800480). I am using external FLASH (MT25QL128ABA1ESE-0SIT) and external SDRAM (AS4C4M16SA-6TIN).
I have ran into two main issues so far:
Here is the layout:
Here are my clock settings:
Any help or guidance is greatly appreciated.
Thank you.
2021-04-17 12:50 AM
I see here more trouble
For test i recomm configure buffer to internal sdram and test ltdc ffunctionality without sdram.
2021-06-26 2:04 AM
d
2021-06-26 2:05 AM
@YTalh.1 (Community Member) Did you solve these issues? If so, can you share how to solve?
2021-12-07 12:57 AM
Hi
could you solve it? would plz chare the solution?