cancel
Showing results for 
Search instead for 
Did you mean: 

F746G-DISC does not work with TouchGfx 4.22.1

hbZhao
Associate III

Hello,

I just bought a STM32F746G-DISCO from Mouser (STM32F746G-DISCO STMicroelectronics | Mouser).

After it arrived, the LCD and touch screen were working well. However, after I downloaded the demo project (STM32F746G-DISCO Control LED from GUI v3.0.6) in the TouchGfx 4.22.1, there is not anything displayed. Also I removed the TouchGfx and installed a version, 4.21.3, but there is not any luck.

 

The board is the blue one. The label on the front is 'STM32F746G-DISCO DK32F746G$CU2', and the label on the back is 'MB1191-F746-C01 / C222103562'.

I found in the previous discussions, the hardware has been changed from version B to version C.

  • QSPI Micron N25Q128A13EF840F changed in MT25QL128ABA1EW9-0SIT (reached B-05)
  • LCD Rocktech RK043FN48H-CT672B changed in KUNJIAN HT043C (reached B-05)
  • MEMS ST MP34DT01TR-M changed in ST IMP34DT05TR (reached C-01)
  • Oscillator NDK NZ2520SB 25MHz END4869B changed in NDK NZ2520SH 25MHz END4869C (reached C-01)
  • Oscillator NDK NZ2520SB 24MHz END4869B changed in NDK NZ2520SH 24MHz END4869D (reached C-01)
  • USB protection ST USBULC6-2F3 changed in ON Semiconductor ESD7383NCTBG (reached C-01)

May I know how to generate a WORKIING project with TouchGFX? Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @hbZhao ,

Sorry for the late response, 
I tried the board specific demo with a MB1191-F746-C01 (I think it's a bit older than the one you have but shouldn't be any drastic changes), and it works correctly. 
Could you please check if you can run other demos (non-board specific ones) on your board? By going in the Demos section and selecting F746 as your Board Setup.

Thank you

Mohammad MORADI
ST Software Developer | TouchGFX

View solution in original post

4 REPLIES 4

Hello @hbZhao ,

Sorry for the late response, 
I tried the board specific demo with a MB1191-F746-C01 (I think it's a bit older than the one you have but shouldn't be any drastic changes), and it works correctly. 
Could you please check if you can run other demos (non-board specific ones) on your board? By going in the Demos section and selecting F746 as your Board Setup.

Thank you

Mohammad MORADI
ST Software Developer | TouchGFX
hbZhao
Associate III

Hello Mohammad MORADI,

 

Thanks for your feedback. This issue has been fixed after I downgraded the development tools.

 

Best Regards

Okay, nice to hear

Good luck

Mohammad MORADI
ST Software Developer | TouchGFX

@hbZhao 
What version did you have to downgrade to? I am currently having this problem.