cancel
Showing results for 
Search instead for 
Did you mean: 

"LTDC" option not available as Application Tick Source in X-CUBE-TOUCHGFX

Ricko
Senior III

Hi,

as you can see in the first screenshot, in the X-CUBE-TOUCHGFX settings (TouchGFX Generator tab) the LTDC option for the Application Tick Source is not available. And at the bottom it says "LTDC in only available if enabled".

LTDC is enabled and configured (second screenshot). Does it need to be configured and/or enabled in some other ways or some other place too?

Thank you :)

 

Ricko_0-1741661353205.png

Ricko_1-1741661458299.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.

View solution in original post

5 REPLIES 5

Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.

Ricko
Senior III

Thank you @jchernus-fikst

but as you can see it is greyed out and cannot be selected. I was asking why and what else I would need to enable in order for it to not be greyed out so I can select it.

Thank you :)

Please re-read my answer.

Your question asked about Driver -> Application Tick Source. I'm suggesting you change Display -> Interface. These are two different things. 

Julia

Sorry @jchernus-fikst long days i front of the PC, I misread your answer.

Yes, now it works.

Thank you! :)

Great! Happy it works, I got stuck on this too just a few weeks ago. Their instructions are not very clear.