cancel
Showing results for 
Search instead for 
Did you mean: 

Errors after generating code with TouchGFX Generator

MLair.1
Associate III

Hello,

I'm using the Mikromedia 7 Capacitive with the STM32F476ZG MCU. I'd like to make an application with TouchGFX.

I followed the Generator User Guide but as soon as I tick Graphics Application from X-CUBE-TOUCHGFX, it generates two errors in app_touchgfx.c (undefined references to touchgfx_init and touchgfx_taskEntry).

Did I forget an important step or is there normal ?

0693W00000D0am3QAB.png0693W00000D0ammQAB.png 

Thanks,

Maël

4 REPLIES 4
MM..1
Chief III

You skip TochGFX designer step, on your second screenshot open Applicatio.template.touchgfx.part file and generate GUI before build

MLair.1
Associate III

I already did that several times, it doesn't change anything of the problem, here is the screenshot you wanted

0693W00000D0ajtQAB.png

MM..1
Chief III

Seems as new bug in 1.7.0 . I dont use new versions because ST sw quality is ...

I hear about missed LIB settings, but not details

MLair.1
Associate III

Yes, it's possible, the fact is I opened a huge project with exactly the same file and it seems to build well. It's confusing..