2021-01-20 3:52 AM
Hi,
In CubeMx, Project Manager tab -> Advanced Settings, the "Do Not Generate Function Call" for MX_TouchGFX_Init is not working.
After selecting it and generating the code, the MX_TouchGFX_Init() is still present in the main.c and going back to the Advanced Settings, the previously selected check box got deselected.
This is a problem because when using the QuadSpi with TouchGFx, it needs to be mapped before TouchGFX initialization.
The mapping cannot be made in the MX_QUADSPI_Init because there is no USER CODE section at the end of this function (Hey ST, what about having a user code section at the end of EVERY HAL init function???).
Settings:
MCU: STM32H743
CubeMx: 6.1.1
CubeIDE: 1.5.1
Firmware Package: FW_H7 1.8.0
Solved! Go to Solution.
2021-01-21 5:58 AM
So I did a bit more testing and this issue seems to happen for all functions from additional X-Cube packages (like X-Cube-TouchGFX, X-CubeBLE, X-CubeNFC4, ...).
I created an internal ticket to investigate and fix this, thank you for reporting this.
2021-01-20 6:12 AM
Hi,
Thank you for reporting this. I am surprised by it as well as I could replicate the issue on projects on a STM32H743 eval board and on a H7b3 dk board. It seems that only the MX_TouchGFX_Init is not working, we will investigate more on that (might be just me not aware of a step to do). Could you add the topic "CubeMX" in the Topic tags of this post ? That way this will have more visibility.
Are you working on a custom board ? Did you start your project from scratch from CubeMX ? I am asking this because from what I understand from your message, you have the MX_TouchGFX_Init called before the MX_QUADSPI_Init ? This is not the case in the application template for the H743 eval board available on TouchGFX Designer. I believe the issue might come in your case from the "rank order" of your functions: you can see that in the Project Manager tab -> Advanced Settings --> Generated Function Calls. You can change the ranks of the function by selecting a function and pressing the "up or low arrows" on the top right (see picture)
/Romain
2021-01-20 6:33 AM
Hi Romain,
Thanks for the answer.
(CubeMX is now added to the topic).
Yes, I am working on a custom board, starting from scratch with CubeMX.
The MX_TouchGFX_Init is indeed called after the MX_QUADSPI_Init.
However, the bit of code to map the QSPI must be after MX_QUADSPI_Init and before MX_TouchGFX_Init.
The best place to add this code would be at the end of the MX_QUADSPI_Init function, but this is not possible because there is no "user code" section there.
What I have done now (and is working) is that I selected the "Do Not Generate Function Call" for the QSPI instead and moved the call to a user code section earlier in the main ("USER CODE BEGIN SysInit"). Then I do the QSPI mapping.
2021-01-21 5:58 AM
So I did a bit more testing and this issue seems to happen for all functions from additional X-Cube packages (like X-Cube-TouchGFX, X-CubeBLE, X-CubeNFC4, ...).
I created an internal ticket to investigate and fix this, thank you for reporting this.
2021-01-21 6:13 AM
Thanks for checking on this issue and creating the ticket!
2021-01-21 8:49 AM
You wrote: "This is a problem because when using the QuadSpi with TouchGFx, it needs to be mapped before TouchGFX initialization."
I tried to make a STM32CubeIDE project for STM32H743 and then enabled QSPI functionality in CubeMX.
At the end (last 2 lines) of MX_QUADSPI_Init() function I can now see the user code section:
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
If you put your QSPI mapping code there it will be called before MX_TouchGFX_Init() is called.
If you don't have these 2 lines, maybe you had deleted them, or you use older fw library (I used STM32Cube_FW_H7_V1.8.0).
2021-01-21 11:08 AM
Hi KPort,
Can you tell me which version of CubeMx you are using?
I do not have any USER CODE BEGIN in the MX_QUADSPI_Init() function (I do have it in the HAL_QSPI_MspInit, but that's not the right place for the mapping code).
I did a test by writing some garbage in this function and refreshing the CubeMx project. It does rewrite the MX_QUADSPI_Init(), but still no user code section
/* QUADSPI init function */
void MX_QUADSPI_Init(void)
{
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 1;
hqspi.Init.FifoThreshold = 4;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE;
hqspi.Init.FlashSize = 23;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
}
2021-01-21 11:11 AM
BTW, my firmware package is FW_H7 V1.8.0.
2021-01-21 12:15 PM
OK, I found out why I don't have a user code section.
It depends if the peripheral initialization is done in the main.c or in separated files.
In CubeMx Project Manager->CodeGenerator->Generated files, if the "Generate peripheral initialization as pair '.c/.h' files per peripheral" is selected, the MX_QUADSPI_Init function does not include the user code sections!
2021-01-21 12:58 PM
Hi franck23,
I'using the latest STM32CubeIDE 1.5.1 and CubeMX 6.1.1 and FW_H7 V1.8.0.
The problem seems to be that you have selected in CubeMX the option "Generate peripheral initialization as a pair of '.c/.h' files per peripheral".
With this option it generates separate .c/.h files for each peripheral AND you don't get all the user code sections.
Without this option selected the generated code for MX_QUADSPI_Init() has all needed user code sections (but the code is inside main.c).
You could do the following: define a macro in main.c just before the HAL initializations like this:
/* USER CODE BEGIN SysInit */
#define MX_QUADSPI_Init() MX_QUADSPI_Init(); map_my_qspi()
/* USER CODE END SysInit */
...where map_my_qspi() is your custom code, run right after MX_QUADSPI_Init() (also declare it in section /* USER CODE BEGIN PFP */).
If you generate the code without the "Generate peripheral initialization..." flag selected, then it all becomes so much easier...
This is what gets generated without the flag (look at... /* USER CODE BEGIN QUADSPI_Init 2 */):
static void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
/* QUADSPI parameter configuration*/
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 255;
hqspi.Init.FifoThreshold = 1;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
hqspi.Init.FlashSize = 1;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
}