Skip to main content
PKunK.1
Associate III
February 3, 2021
Question

How to use ILI9806E as a 5-inch MIPI interface on the stm32f469i_Discoveryboard?

  • February 3, 2021
  • 0 replies
  • 589 views

We are going to test it by changing the LCD on the stm32f469i_Discoveryboard.

The 5-inch LCD has a resolution of 855×480, and the Control IC is an ILI9806E

The control method is to use the MIPI interface, but I couldn't find the driver information for the ILI9806E.

If anyone has worked on it, can you share the information?

This topic has been closed for replies.