2021-05-21 8:23 AM
Hello!
We are use STM32H747 and TouchGFX. We are need to use DMA2D. But we have issue with mode DMA2D_R2M.
Our configuration
hdma2d.Instance = DMA2D;
hdma2d.Init.Mode = DMA2D_R2M;
hdma2d.Init.ColorMode = DMA2D_OUTPUT_ARGB8888;
hdma2d.Init.OutputOffset = 0;
if (HAL_DMA2D_Init(&hdma2d) != HAL_OK)
{
while (1);
}
if (HAL_DMA2D_ConfigLayer(&hdma2d, 1) != HAL_OK)
{
while (1);
}
Our test
NVIC_EnableIRQ(DMA2D_IRQn);
HAL_DMA2D_Start_IT(&hdma2d, 0x12345678, 0xD0165800, 640, 572);
In this case we have callback from DMA with configuration error.
For mode DMA2D_R2M - all Ok.
Any ideas?
Solved! Go to Solution.
2021-05-28 1:34 AM
Thanks for answer!
But I found that for hdma2d.Init.Mode = DMA2D_R2M function HAL_DMA2D_Init (...) set into CR mode as 0x07, not 0x03.
I updated code for correct mode and now all works!
2021-05-27 8:10 AM
Hello @Community member ,
Have a look at the "Configuration error detection" subchapter of DMA2D chapter in the RM0399, and check with the condition and configuration that you have.
Hope this helps you :smiling_face_with_smiling_eyes: !
Please mark my answer as best by clicking on the "Select as Best" button if it helped.
Imen
2021-05-28 1:34 AM
Thanks for answer!
But I found that for hdma2d.Init.Mode = DMA2D_R2M function HAL_DMA2D_Init (...) set into CR mode as 0x07, not 0x03.
I updated code for correct mode and now all works!
2021-05-28 1:40 AM
Thanks for sharing the update and your solution!
I'm really glad to know you overcame this problem :)
Imen