Display flickering STM32F746
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-03 11:18 PM
Hello, I am using STM32F746 with FMC SDRAM, QSPI flash, DMA2D. I observed my display is flicking. You can check video using below link.
https://drive.google.com/file/d/1j3uyyHWHlFO-fGW23RI33Iyos6meYaB-/view?usp=sharing
Any suggestions for solving this issue.
I am using custom board with MCU 746 with below software with version :
- Touchgfx 4.15.0
- CubeMX 5.4.0
- IDE : System workbench for STM32
Thanks
- Labels:
-
STM32CubeMX
-
STM32F7 Series
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-05 4:51 AM
@Alexandre RENOUX @EEuge
I updated both touch gfx and stm32cubmx. I am using stmcube Ide now.
During compilation I am getting 2 _sbrk function. One in syacall.c and another in sysmem.c . Don't know which should I use.
syacall.c :
addr_t _sbrk(int incr)
{
extern char end asm("end");
static char *heap_end;
char *prev_heap_end;
if (heap_end == 0)
heap_end = &end;
prev_heap_end = heap_end;
if (heap_end + incr > stack_ptr)
{
// write(1, "Heap and stack collision\n", 25);
// abort();
errno = ENOMEM;
return (caddr_t) -1;
}
heap_end += incr;
return (caddr_t) prev_heap_end;
}
sysmem.c
void *_sbrk(ptrdiff_t incr)
{
extern uint8_t _end; /* Symbol defined in the linker script */
extern uint8_t _estack; /* Symbol defined in the linker script */
extern uint32_t _Min_Stack_Size; /* Symbol defined in the linker script */
const uint32_t stack_limit = (uint32_t)&_estack - (uint32_t)&_Min_Stack_Size;
const uint8_t *max_heap = (uint8_t *)stack_limit;
uint8_t *prev_heap_end;
/* Initialize heap end at first call */
if (NULL == __sbrk_heap_end)
{
__sbrk_heap_end = &_end;
}
/* Protect heap from growing into the reserved MSP stack */
if (__sbrk_heap_end + incr > max_heap)
{
errno = ENOMEM;
return (void *)-1;
}
prev_heap_end = __sbrk_heap_end;
__sbrk_heap_end += incr;
return (void *)prev_heap_end;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-05 5:07 AM
Also frameBuf, It should got to external RAM so i create a session in linker and place it like below:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
EXRAM (rx) : ORIGIN = 0x20000000, LENGTH = 8M
}
ExtFlashSection :
{
. = ALIGN(4);
*(TouchGFX_Framebuffer TouchGFX_Framebuffer.*)
. = ALIGN(4);
} >EXRAM
but also this big wouldn't fit in 8MB. Something seems wrong. I am using RGB565.
Also in new code i can't find below functions. Do I need to add it manually ?
/* Initialise the graphical hardware */
GRAPHICS_HW_Init();
/* Initialise the graphical stack engine */
GRAPHICS_Init();
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-05 10:52 PM
@Alexandre RENOUX
Hello, I am testing the code but now its going for hard fault post prvPortStartFirstTask().
I checked fault register CFSR value, its 0x400.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-05 11:01 PM
Hello,
Did you refer to the F746-DISCO Application Template ? I feel like so many things can be wrong in your code so I suggest you to start fresh from the F746-DISCO Application template and modify the parts that are necessary (from what I can see your project is very similar to the F746-DISCO so I believe only a few things need to be changed). What's your display interface ? If it is LTDC, then just modifying the LTDC settings in CubeMX should be sufficient.
/Alexandre
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-05 11:03 PM
YES, Its LTDC interface. My chip package is different than discovery board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-06 2:19 AM
@Alexandre RENOUX @EEuge
I successfully updated to latest version but still display only get hanged like above image after soometimes, STM is working fine. When I Reset disp pin of display (out of 40 pin) , display starts working again.
Any suggestions from your side?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-06 6:08 PM
Hi,
If you based yourself upon the F746-DISCO Application Template and when debugging, the STM is working correctly while the display freezes, then maybe the problem is your display. In this case, you need to contact the display provider because this is outside the scope of ST.
/Alexandre
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-06 9:16 PM
@Alexandre RENOUX
Hi, It seems like some setting issue to me. Attaching one video. Please see if this can guess any thing.
https://drive.google.com/file/d/1aHzFAm7nPRnVgXYCEWYI4O2yCz6481Zk/view?usp=sharing
Also one doubt, For updating display we send data mode.cpp -> presenter.cpp -> view.cpp and we passed data in function input. Suppose rather than sending function input, if I just send void in all functions and in view.cpp function use some global variable of other file to update display. Is this fine?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-07 6:25 AM
@Alexandre RENOUX I created one thread related to issue. Please check.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-08 12:39 PM
I see, you didn't followed my advise?
- lockDMAToFrontPorch(false); set it to true!