2021-11-18 03:45 AM
I am using STMCubeIDE 1.7.0 on linux computer and running designer on windows host as virtual machine ...
Is that maybe the problem, that I have to expose some directories from CubeIDE?
Or is it from now on "only-simulator/no-boards" a proper reality?
If I remember correctly with v4.16 I could select boards without any problem...
Is there any clue about it?
Thanks, Ziga
2021-12-16 02:39 AM
The same is with v18.1....
What is the dependency to get boards/demos/example to be loaded?
(Internet is available ... any other?)
What am I doing wrong here, I don't understand?
Thanks for any info,
BR